<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックMultiple timer functions in same FTM</title>
    <link>https://community.nxp.com/t5/S32K/Multiple-timer-functions-in-same-FTM/m-p/2028985#M45166</link>
    <description>&lt;P&gt;I want to use one FTM channel as PWM output, and another one for IC, both signals are the same frequency so, the MOD register wont be an issue.&lt;BR /&gt;&lt;BR /&gt;Basically I want to compare the output PWM with what is being captured, this signal goes through other boards and eventually comes back.&lt;BR /&gt;Is there a way of checking that the period and phase are the same?&lt;BR /&gt;Right now I cannot configure the FTM to work in both modes. Also, I know FTM doesn't support phase comparison but I found a workaround for that one.&lt;BR /&gt;&lt;BR /&gt;I have read this, but this one if for OC mode:&amp;nbsp;&lt;A title="Use-an-FTM-IC-device-to-set-several-channels-as-output-compare" href="https://community.nxp.com/t5/S32K/Use-an-FTM-IC-device-to-set-several-channels-as-output-compare/m-p/1293212" target="_blank" rel="noopener"&gt;Use-an-FTM-IC-device-to-set-several-channels-as-output-compare&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 11:09:50 GMT</pubDate>
    <dc:creator>Mudkip</dc:creator>
    <dc:date>2025-01-16T11:09:50Z</dc:date>
    <item>
      <title>Multiple timer functions in same FTM</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-timer-functions-in-same-FTM/m-p/2028985#M45166</link>
      <description>&lt;P&gt;I want to use one FTM channel as PWM output, and another one for IC, both signals are the same frequency so, the MOD register wont be an issue.&lt;BR /&gt;&lt;BR /&gt;Basically I want to compare the output PWM with what is being captured, this signal goes through other boards and eventually comes back.&lt;BR /&gt;Is there a way of checking that the period and phase are the same?&lt;BR /&gt;Right now I cannot configure the FTM to work in both modes. Also, I know FTM doesn't support phase comparison but I found a workaround for that one.&lt;BR /&gt;&lt;BR /&gt;I have read this, but this one if for OC mode:&amp;nbsp;&lt;A title="Use-an-FTM-IC-device-to-set-several-channels-as-output-compare" href="https://community.nxp.com/t5/S32K/Use-an-FTM-IC-device-to-set-several-channels-as-output-compare/m-p/1293212" target="_blank" rel="noopener"&gt;Use-an-FTM-IC-device-to-set-several-channels-as-output-compare&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 11:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-timer-functions-in-same-FTM/m-p/2028985#M45166</guid>
      <dc:creator>Mudkip</dc:creator>
      <dc:date>2025-01-16T11:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple timer functions in same FTM</title>
      <link>https://community.nxp.com/t5/S32K/Multiple-timer-functions-in-same-FTM/m-p/2029968#M45220</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;I must admit that it is not completely clear your request. What do you mean with checking the phase?&lt;/P&gt;
&lt;P&gt;The FTM capture mode can determine the pulse width or the period of the tested signal but not both of them at the same time.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 21:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Multiple-timer-functions-in-same-FTM/m-p/2029968#M45220</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-01-17T21:00:45Z</dc:date>
    </item>
  </channel>
</rss>