<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flashing Custom S32k144 board using Open SDA Interface in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Flashing-Custom-S32k144-board-using-Open-SDA-Interface/m-p/2028601#M45134</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please see PEMicro's explanation for this:&amp;nbsp;&amp;nbsp;&lt;A href="https://www.pemicro.com/forums/forum_topic.cfm?forum_id=8&amp;amp;forum_topic_id=7505" target="_self"&gt;Program/Debug issue with S32K142-Q48&lt;/A&gt;&lt;FONT color="#666699"&gt;: &lt;FONT color="#808080"&gt;Our OpenSDA interfaces are designed for evaluation purposes to debug and program the onboard target devices. They are not meant to be used to debug devices on external custom boards.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 01:04:20 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-01-16T01:04:20Z</dc:date>
    <item>
      <title>Flashing Custom S32k144 board using Open SDA Interface</title>
      <link>https://community.nxp.com/t5/S32K/Flashing-Custom-S32k144-board-using-Open-SDA-Interface/m-p/2028178#M45117</link>
      <description>&lt;P&gt;I am using the S32K144 evaluation board and would like to flash my custom board using the onboard debugger. I plan to use only the J106 (SWD DIO) and J8 (SWD CLK) pins for this purpose. However, I’ve seen community posts suggesting the use of the J14 10-pin header for flashing. Can I avoid using the J14 header and proceed with just the two pins? Is this approach possible?&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jan 2025 09:27:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flashing-Custom-S32k144-board-using-Open-SDA-Interface/m-p/2028178#M45117</guid>
      <dc:creator>Jeevansagar</dc:creator>
      <dc:date>2025-01-15T09:27:10Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing Custom S32k144 board using Open SDA Interface</title>
      <link>https://community.nxp.com/t5/S32K/Flashing-Custom-S32k144-board-using-Open-SDA-Interface/m-p/2028601#M45134</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please see PEMicro's explanation for this:&amp;nbsp;&amp;nbsp;&lt;A href="https://www.pemicro.com/forums/forum_topic.cfm?forum_id=8&amp;amp;forum_topic_id=7505" target="_self"&gt;Program/Debug issue with S32K142-Q48&lt;/A&gt;&lt;FONT color="#666699"&gt;: &lt;FONT color="#808080"&gt;Our OpenSDA interfaces are designed for evaluation purposes to debug and program the onboard target devices. They are not meant to be used to debug devices on external custom boards.&lt;/FONT&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 01:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flashing-Custom-S32k144-board-using-Open-SDA-Interface/m-p/2028601#M45134</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-01-16T01:04:20Z</dc:date>
    </item>
  </channel>
</rss>