<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K146 external RAM support</title>
    <link>https://community.nxp.com/t5/S32K/S32K146-external-RAM-support/m-p/2027519#M45085</link>
    <description>&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are working with NXPS32K146 chip. Currently, we are using complete SRAM for our application and can not add more features after that due to limited RAM space.&lt;BR /&gt;&lt;BR /&gt;Can We solder external RAM and use along with SRAM?&lt;BR /&gt;Can We replace the complete SRAM with double size?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any alternative solution to increase SRAM without chip up?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and best Regards,&lt;/P&gt;&lt;P&gt;Sai&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K146EVB" id="S32K146EVB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="S32K148-T-BOX" id="S32K148-T-BOX"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 14 Jan 2025 10:18:59 GMT</pubDate>
    <dc:creator>saireddy_saredd</dc:creator>
    <dc:date>2025-01-14T10:18:59Z</dc:date>
    <item>
      <title>S32K146 external RAM support</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-external-RAM-support/m-p/2027519#M45085</link>
      <description>&lt;P&gt;Hallo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are working with NXPS32K146 chip. Currently, we are using complete SRAM for our application and can not add more features after that due to limited RAM space.&lt;BR /&gt;&lt;BR /&gt;Can We solder external RAM and use along with SRAM?&lt;BR /&gt;Can We replace the complete SRAM with double size?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are there any alternative solution to increase SRAM without chip up?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and best Regards,&lt;/P&gt;&lt;P&gt;Sai&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="S32K146EVB" id="S32K146EVB"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;LI-PRODUCT title="S32K148-T-BOX" id="S32K148-T-BOX"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Jan 2025 10:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-external-RAM-support/m-p/2027519#M45085</guid>
      <dc:creator>saireddy_saredd</dc:creator>
      <dc:date>2025-01-14T10:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K146 external RAM support</title>
      <link>https://community.nxp.com/t5/S32K/S32K146-external-RAM-support/m-p/2029326#M45183</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;For S32K146 you have 128KB as SRAM and also you can use 4 KB of FlexRAM for use as SRAM too. Additionally, such S32K1 derivative do not have External memory interface (Please refer to &lt;EM&gt;Feature comparison&lt;/EM&gt;&amp;nbsp;section of datasheet).&lt;/P&gt;
&lt;P&gt;So your best option is to upgrade to another S32K1 derivative, like K148.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 22:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K146-external-RAM-support/m-p/2029326#M45183</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2025-01-16T22:55:46Z</dc:date>
    </item>
  </channel>
</rss>