<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32 K118 Internal clock Lin</title>
    <link>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2026230#M45026</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Jianfeng2,&lt;/P&gt;
&lt;P&gt;If you are using S32K1 SDK, please check if "&lt;STRONG&gt;START_FROM_FLASH&lt;/STRONG&gt;" Symbols are missing? refer to the discussion:&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/td-p/1203150" target="_self"&gt;S32K188 runs with debugger, but not witout&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you suspect the clock is inaccurate, please observe the frequency of internal clock through the CLKOUT pin.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jan 2025 00:48:54 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2025-01-13T00:48:54Z</dc:date>
    <item>
      <title>S32 K118 Internal clock Lin</title>
      <link>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2025686#M44996</link>
      <description>&lt;P&gt;I use S32k118, there is no external crystal oscillator, so i use internal clock.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The problem is that the system is works fine in debug mode.&amp;nbsp; And If power off, then power on, it can't run normally.&lt;/P&gt;&lt;P&gt;Attached is the clock config. Is there anything special when use internal clock? Could you give me some supports?&lt;/P&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;</description>
      <pubDate>Fri, 10 Jan 2025 09:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2025686#M44996</guid>
      <dc:creator>Jianfeng2</dc:creator>
      <dc:date>2025-01-10T09:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32 K118 Internal clock Lin</title>
      <link>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2026230#M45026</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Jianfeng2,&lt;/P&gt;
&lt;P&gt;If you are using S32K1 SDK, please check if "&lt;STRONG&gt;START_FROM_FLASH&lt;/STRONG&gt;" Symbols are missing? refer to the discussion:&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K188-runs-with-debugger-but-not-witout/td-p/1203150" target="_self"&gt;S32K188 runs with debugger, but not witout&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you suspect the clock is inaccurate, please observe the frequency of internal clock through the CLKOUT pin.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 00:48:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2026230#M45026</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2025-01-13T00:48:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32 K118 Internal clock Lin</title>
      <link>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2026420#M45034</link>
      <description>&lt;P&gt;Solved, Thank you very much!&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 06:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32-K118-Internal-clock-Lin/m-p/2026420#M45034</guid>
      <dc:creator>Jianfeng2</dc:creator>
      <dc:date>2025-01-13T06:04:25Z</dc:date>
    </item>
  </channel>
</rss>