<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K312 LIN LPUART_LIN_IP_RX_OVERRUN_ERROR in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-LIN-LPUART-LIN-IP-RX-OVERRUN-ERROR/m-p/2024548#M44938</link>
    <description>&lt;P&gt;Hello everyone:&lt;/P&gt;&lt;P&gt;I tried to use S23K312 for Ip Lin debugging with Baby Lin II.&lt;/P&gt;&lt;P&gt;Whether I use slave mode or master mode, I get LPUART_LIN_IP_RX_OVERRUN_ERROR, and even LPUART_LIN_IP_FRAME_ERROR and LPUART_LIN_IP_PID_ERROR.&lt;/P&gt;&lt;P&gt;I also tried to change the bit rate, such as 19200 or 9600, but nothing seemed to work.&lt;/P&gt;&lt;P&gt;Attached are screenshots of the engineering and debugging I used.&lt;/P&gt;&lt;P&gt;Please help me confirm what my problem is.&lt;/P&gt;&lt;P&gt;Also, please help me explain what each error in the enum type Lpuart_Lin_Ip_EventIdType means, as I feel the remarks about it are unclear.&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jan 2025 06:41:22 GMT</pubDate>
    <dc:creator>jichengyou</dc:creator>
    <dc:date>2025-01-09T06:41:22Z</dc:date>
    <item>
      <title>S32K312 LIN LPUART_LIN_IP_RX_OVERRUN_ERROR</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LIN-LPUART-LIN-IP-RX-OVERRUN-ERROR/m-p/2024548#M44938</link>
      <description>&lt;P&gt;Hello everyone:&lt;/P&gt;&lt;P&gt;I tried to use S23K312 for Ip Lin debugging with Baby Lin II.&lt;/P&gt;&lt;P&gt;Whether I use slave mode or master mode, I get LPUART_LIN_IP_RX_OVERRUN_ERROR, and even LPUART_LIN_IP_FRAME_ERROR and LPUART_LIN_IP_PID_ERROR.&lt;/P&gt;&lt;P&gt;I also tried to change the bit rate, such as 19200 or 9600, but nothing seemed to work.&lt;/P&gt;&lt;P&gt;Attached are screenshots of the engineering and debugging I used.&lt;/P&gt;&lt;P&gt;Please help me confirm what my problem is.&lt;/P&gt;&lt;P&gt;Also, please help me explain what each error in the enum type Lpuart_Lin_Ip_EventIdType means, as I feel the remarks about it are unclear.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 06:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LIN-LPUART-LIN-IP-RX-OVERRUN-ERROR/m-p/2024548#M44938</guid>
      <dc:creator>jichengyou</dc:creator>
      <dc:date>2025-01-09T06:41:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 LIN LPUART_LIN_IP_RX_OVERRUN_ERROR</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-LIN-LPUART-LIN-IP-RX-OVERRUN-ERROR/m-p/2035131#M45491</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194912"&gt;@jichengyou&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Based on our discussion in a support ticket, the last problem with LPUART_LIN_IP_STATUS_TX_BUSY after SYNC has been send can be caused by an issue in the HW of the tranceiver, because it occurs after Power-on reset.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jan 2025 13:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-LIN-LPUART-LIN-IP-RX-OVERRUN-ERROR/m-p/2035131#M45491</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-01-28T13:58:33Z</dc:date>
    </item>
  </channel>
</rss>