<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144EVB-Q100 LIN in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022577#M44822</link>
    <description>&lt;P&gt;Hi Tereza,&lt;/P&gt;
&lt;P&gt;seems you must have some older board, probably FRDMPK144, where MCZ33903 is used. On&amp;nbsp;&lt;BR /&gt;new one simple TJA1027 is used as LIN transceiver. RTD demo does not cover MCZ33903 and seems you will need to enable internal LIN transceiver &amp;amp; LIN termination to make example functional.&lt;BR /&gt;Below AN could help I think,&amp;nbsp;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4770.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4770.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 06 Jan 2025 12:24:54 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2025-01-06T12:24:54Z</dc:date>
    <item>
      <title>S32K144EVB-Q100 LIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022133#M44791</link>
      <description>&lt;P&gt;I have a S32K144EVB-Q100 board that has a MCZ33903 SBC that supports LIN. I would like to use it in an application, but I cannot seem to make the LIN example (Lin_Lpuart_MasterFrameTransfer_S32K144) work. It always ends with a timeout and the T_LinStatus remains in LIN_TX_BUSY. If I look at the LIN_TX line going to the SBC, I can see the sync and the break field get transmitted, but it never transmits the PID.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2025-01-05 175857.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318113i3B08F18358039173/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2025-01-05 175857.png" alt="Screenshot 2025-01-05 175857.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;In the code, the LinCurrentState-&amp;gt;CurrentNodeState gets set to LPUART_LIN_IP_NODE_STATE_SEND_SYNC but the Lpuart_Lin_Ip_FrameIrqHandler newer gets called afterwards.&lt;/P&gt;
&lt;P&gt;I am assuming that no external connections are needed as there's nothing written in the description file.&lt;/P&gt;
&lt;P&gt;Does anyone know what might be causing this?&lt;/P&gt;
&lt;P&gt;I am using S32DS 3.5 and S32K1_S32M24X Real-Time Drivers Version2.0.0.&lt;/P&gt;</description>
      <pubDate>Sun, 05 Jan 2025 16:59:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022133#M44791</guid>
      <dc:creator>tkubincova</dc:creator>
      <dc:date>2025-01-05T16:59:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 LIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022577#M44822</link>
      <description>&lt;P&gt;Hi Tereza,&lt;/P&gt;
&lt;P&gt;seems you must have some older board, probably FRDMPK144, where MCZ33903 is used. On&amp;nbsp;&lt;BR /&gt;new one simple TJA1027 is used as LIN transceiver. RTD demo does not cover MCZ33903 and seems you will need to enable internal LIN transceiver &amp;amp; LIN termination to make example functional.&lt;BR /&gt;Below AN could help I think,&amp;nbsp;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN4770.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4770.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jan 2025 12:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022577#M44822</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-01-06T12:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 LIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022637#M44825</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I found another one that should have TJA1027, but the problem is the same&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2025-01-05 161140.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318242i0D84043F1DBBB631/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2025-01-05 161140.png" alt="Screenshot 2025-01-05 161140.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;the break and sync get sent, but nothing else and the example results in timeout.&lt;/P&gt;
&lt;P&gt;I cannot find the schematic for the SCH-29248 REV A board, but it's visible that the TJA1027 is there&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Media (2).jpg" style="width: 225px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318244i8AD757DC32295F1E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Media (2).jpg" alt="Media (2).jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Media (1).jpg" style="width: 225px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/318243iDF5D4F21BBB33473/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Media (1).jpg" alt="Media (1).jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jan 2025 15:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2022637#M44825</guid>
      <dc:creator>tkubincova</dc:creator>
      <dc:date>2025-01-06T15:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144EVB-Q100 LIN</title>
      <link>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2023327#M44863</link>
      <description>&lt;P&gt;Hi Tereza,&lt;/P&gt;
&lt;P&gt;unfortunately I do not have revA schematic, try revB, it would be similar,&amp;nbsp;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K144EVB-SCH-29248-RB" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K144EVB-SCH-29248-RB&lt;/A&gt;&lt;BR /&gt;Still this looks some very old board, probably with preproduction device. I can recommend to get some new one.&lt;BR /&gt;Anyway you need to power board with external 12V so TJA1027 will be powered, and be sure its /SLP pin is held high so transceiver is in Normal mode.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jan 2025 13:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144EVB-Q100-LIN/m-p/2023327#M44863</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-01-07T13:45:17Z</dc:date>
    </item>
  </channel>
</rss>