<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k144 Adc Triggering using FTM in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k144-Adc-Triggering-using-FTM/m-p/2022553#M44818</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213140"&gt;@Jeevansagar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The FTM module provides two triggers, on Initialization and External trigger on match - but this is when the PWM signal toggles.&lt;/P&gt;
&lt;P&gt;1.&lt;/P&gt;
&lt;P&gt;If you need to delay the trigger, there is the PDB for that purpose. You can refer to the S32K144 Motor control demos: &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK144" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK144&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2.&lt;/P&gt;
&lt;P&gt;The PDB interrupt can be used to count the cycles. And the PDB channel that triggers the ADC every 10 cycle can be dynamically enabled and disbabled (PDB_CHnC1).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
    <pubDate>Mon, 06 Jan 2025 11:44:37 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2025-01-06T11:44:37Z</dc:date>
    <item>
      <title>S32k144 Adc Triggering using FTM</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-Adc-Triggering-using-FTM/m-p/2021656#M44754</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am working with the NXP S32K144 microcontroller and need help configuring ADC triggering. I am using the FTM3 module to generate a 10 kHz PWM signal, which also provides an initialization trigger when the counter reaches the MOD value.&lt;BR /&gt;&lt;BR /&gt;I am utilizing both ADC modules (ADC0 and ADC1) and have the following requirements:&lt;BR /&gt;&lt;BR /&gt;1. ADC0 should be triggered at every PWM cycle (10 kHz) but at the peak or trough of the PWM signal, avoiding triggers during the rising or falling edges.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;2. ADC1 should be triggered at 1 kHz (every 10 PWM cycles) and also avoid being triggered near the PWM edges.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Is there a way to achieve this configuration using the FTM3 or PDB modules? Any guidance or examples would be appreciated.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 06:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-Adc-Triggering-using-FTM/m-p/2021656#M44754</guid>
      <dc:creator>Jeevansagar</dc:creator>
      <dc:date>2025-01-03T06:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32k144 Adc Triggering using FTM</title>
      <link>https://community.nxp.com/t5/S32K/S32k144-Adc-Triggering-using-FTM/m-p/2022553#M44818</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213140"&gt;@Jeevansagar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The FTM module provides two triggers, on Initialization and External trigger on match - but this is when the PWM signal toggles.&lt;/P&gt;
&lt;P&gt;1.&lt;/P&gt;
&lt;P&gt;If you need to delay the trigger, there is the PDB for that purpose. You can refer to the S32K144 Motor control demos: &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK144" target="_blank"&gt;https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK144&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2.&lt;/P&gt;
&lt;P&gt;The PDB interrupt can be used to count the cycles. And the PDB channel that triggers the ADC every 10 cycle can be dynamically enabled and disbabled (PDB_CHnC1).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 06 Jan 2025 11:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k144-Adc-Triggering-using-FTM/m-p/2022553#M44818</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2025-01-06T11:44:37Z</dc:date>
    </item>
  </channel>
</rss>