<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k312 flexcan</title>
    <link>https://community.nxp.com/t5/S32K/s32k312-flexcan/m-p/2021324#M44720</link>
    <description>&lt;P&gt;Dear NXP engineers, I am encountering an issue when using FlexCAN to periodically send CAN messages. For instance, when I attempt to send over 10 CAN frames within a 50ms period, I notice significant deviations in the reception times of these CAN data, with some deviations even reaching around 4ms. Specifically, I am sending CAN messages in the following manner within my task period:&lt;/P&gt;&lt;P&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb9, &amp;amp;CAN_NODE_0_TX_STD_Config, 0x01, mb_data);&lt;BR /&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb10, &amp;amp;CAN_NODE_0_TX_STD_Config, 0x02, mb_data);&lt;BR /&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb11 &amp;amp;CAN_NODE_0_TX_STD_Config, 0x03, mb_data);&lt;BR /&gt;.....&lt;BR /&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb18 &amp;amp;CAN_NODE_0_TX_STD_Config, 0x10, mb_data);&lt;/P&gt;&lt;P&gt;Could you please provide some insights on this matter?&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jan 2025 14:03:10 GMT</pubDate>
    <dc:creator>fengba_360</dc:creator>
    <dc:date>2025-01-02T14:03:10Z</dc:date>
    <item>
      <title>s32k312 flexcan</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flexcan/m-p/2021324#M44720</link>
      <description>&lt;P&gt;Dear NXP engineers, I am encountering an issue when using FlexCAN to periodically send CAN messages. For instance, when I attempt to send over 10 CAN frames within a 50ms period, I notice significant deviations in the reception times of these CAN data, with some deviations even reaching around 4ms. Specifically, I am sending CAN messages in the following manner within my task period:&lt;/P&gt;&lt;P&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb9, &amp;amp;CAN_NODE_0_TX_STD_Config, 0x01, mb_data);&lt;BR /&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb10, &amp;amp;CAN_NODE_0_TX_STD_Config, 0x02, mb_data);&lt;BR /&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb11 &amp;amp;CAN_NODE_0_TX_STD_Config, 0x03, mb_data);&lt;BR /&gt;.....&lt;BR /&gt;FlexCAN_Ip_Send(CAN_NODE_0, mb18 &amp;amp;CAN_NODE_0_TX_STD_Config, 0x10, mb_data);&lt;/P&gt;&lt;P&gt;Could you please provide some insights on this matter?&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jan 2025 14:03:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flexcan/m-p/2021324#M44720</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2025-01-02T14:03:10Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 flexcan</title>
      <link>https://community.nxp.com/t5/S32K/s32k312-flexcan/m-p/2021782#M44767</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;possible root cause could be interrupt processing, which could delay MB preparation for transmission. Can be other modules interrupts or also FlexCAN ISR itself. After successful transmission MB interrupt is called, assuming polling mode is not used.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 09:09:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k312-flexcan/m-p/2021782#M44767</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2025-01-03T09:09:19Z</dc:date>
    </item>
  </channel>
</rss>