<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PE Micro interface settings issue in debug configurations of S32K3X8 289 Eval board in S32K</title>
    <link>https://community.nxp.com/t5/S32K/PE-Micro-interface-settings-issue-in-debug-configurations-of/m-p/2020695#M44670</link>
    <description>&lt;P&gt;Hi, I am using &lt;STRONG&gt;S32K3X8-289 eval board&lt;/STRONG&gt; for debugging purposes. While choosing the interface in PE Micro debugger window, I observe that for a particular hardware interface, all the available interfaces work, and the debugging is successful which should not be the case ideally. For example, if I connect via &lt;STRONG&gt;Multilink USB&lt;/STRONG&gt;, the interface chosen in the configuration should be &lt;STRONG&gt;USB Multilink, USB Multilink FX&lt;/STRONG&gt;, but when I choose any of the available interfaces, the debugging is successful. I tried this with &lt;STRONG&gt;OpenSDA USB&lt;/STRONG&gt; also and the observations were same. Can anyone explain why this is happening or what am I missing in this, as a debugging session should be successful only with the corresponding interface settings only.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Varsha&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2024-12-31 113427.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/317712i541DF3A291159009/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2024-12-31 113427.png" alt="Screenshot 2024-12-31 113427.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2024-12-31 113427.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 31 Dec 2024 06:24:19 GMT</pubDate>
    <dc:creator>rvarsha</dc:creator>
    <dc:date>2024-12-31T06:24:19Z</dc:date>
    <item>
      <title>PE Micro interface settings issue in debug configurations of S32K3X8 289 Eval board</title>
      <link>https://community.nxp.com/t5/S32K/PE-Micro-interface-settings-issue-in-debug-configurations-of/m-p/2020695#M44670</link>
      <description>&lt;P&gt;Hi, I am using &lt;STRONG&gt;S32K3X8-289 eval board&lt;/STRONG&gt; for debugging purposes. While choosing the interface in PE Micro debugger window, I observe that for a particular hardware interface, all the available interfaces work, and the debugging is successful which should not be the case ideally. For example, if I connect via &lt;STRONG&gt;Multilink USB&lt;/STRONG&gt;, the interface chosen in the configuration should be &lt;STRONG&gt;USB Multilink, USB Multilink FX&lt;/STRONG&gt;, but when I choose any of the available interfaces, the debugging is successful. I tried this with &lt;STRONG&gt;OpenSDA USB&lt;/STRONG&gt; also and the observations were same. Can anyone explain why this is happening or what am I missing in this, as a debugging session should be successful only with the corresponding interface settings only.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Varsha&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2024-12-31 113427.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/317712i541DF3A291159009/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot 2024-12-31 113427.png" alt="Screenshot 2024-12-31 113427.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot 2024-12-31 113427.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 31 Dec 2024 06:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/PE-Micro-interface-settings-issue-in-debug-configurations-of/m-p/2020695#M44670</guid>
      <dc:creator>rvarsha</dc:creator>
      <dc:date>2024-12-31T06:24:19Z</dc:date>
    </item>
  </channel>
</rss>