<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 AES encryption performance test</title>
    <link>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2020172#M44640</link>
    <description>&lt;P&gt;Hello, nxp&lt;/P&gt;&lt;P&gt;I would like to measure the AES cryptographic performance of HSM.&lt;BR /&gt;For the three main modes of AES, ECB, CBC, and CTR, I want to encrypt and decrypt data of various lengths to measure the time it takes each, and I wonder if HSE provides a timer or API that can be used to measure the time.&lt;BR /&gt;For example, I would like to check if there is a built-in timer function that can measure the time before and after the AES encryption/decryption function call, or if there is an API that supports it.&lt;/P&gt;&lt;P&gt;If HSE itself does not provide timer functionality, I would also appreciate it if you could let me know if there is any performance measurement method recommended by NXP platform (e.g. using specific MCU timer, using debugging tool, etc.).&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Sun, 29 Dec 2024 10:37:09 GMT</pubDate>
    <dc:creator>minjaekang99</dc:creator>
    <dc:date>2024-12-29T10:37:09Z</dc:date>
    <item>
      <title>AES encryption performance test</title>
      <link>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2020172#M44640</link>
      <description>&lt;P&gt;Hello, nxp&lt;/P&gt;&lt;P&gt;I would like to measure the AES cryptographic performance of HSM.&lt;BR /&gt;For the three main modes of AES, ECB, CBC, and CTR, I want to encrypt and decrypt data of various lengths to measure the time it takes each, and I wonder if HSE provides a timer or API that can be used to measure the time.&lt;BR /&gt;For example, I would like to check if there is a built-in timer function that can measure the time before and after the AES encryption/decryption function call, or if there is an API that supports it.&lt;/P&gt;&lt;P&gt;If HSE itself does not provide timer functionality, I would also appreciate it if you could let me know if there is any performance measurement method recommended by NXP platform (e.g. using specific MCU timer, using debugging tool, etc.).&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Sun, 29 Dec 2024 10:37:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2020172#M44640</guid>
      <dc:creator>minjaekang99</dc:creator>
      <dc:date>2024-12-29T10:37:09Z</dc:date>
    </item>
    <item>
      <title>Re: AES encryption performance test</title>
      <link>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2020562#M44659</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please reply to anyone.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Dec 2024 20:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2020562#M44659</guid>
      <dc:creator>minjaekang99</dc:creator>
      <dc:date>2024-12-30T20:19:58Z</dc:date>
    </item>
    <item>
      <title>Re: AES encryption performance test</title>
      <link>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2021649#M44751</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242600"&gt;@minjaekang99&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;No, HSE does not have a timer or API which could be used for performance monitoring.&lt;/P&gt;
&lt;P&gt;The easiest method is to toggle a pin before and after calling a service and then simply measure the time by an oscilloscope. It's probably the most effective method taking minimal effort.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 03 Jan 2025 06:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AES-encryption-performance-test/m-p/2021649#M44751</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2025-01-03T06:18:56Z</dc:date>
    </item>
  </channel>
</rss>