<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 CAN communication in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019443#M44593</link>
    <description>&lt;P&gt;Hi@&lt;SPAN&gt;Voledi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;S32K3X4-T172 and S32K3X4-Q172 are different, and the CAN transceiver are different.&lt;/P&gt;
&lt;P&gt;This demo is based on S32K3X4-Q172, and the transceiver used is TJA1153.&lt;/P&gt;
&lt;P&gt;And this demo is based on S32 DS V3.4+ RTD 2.0.0, which is not compatible with the version you are using.&lt;/P&gt;
&lt;P&gt;The attached is a routine based on &lt;STRONG&gt;S32K311&lt;/STRONG&gt;, you can refer to it, the version is consistent with what you are currently using.&lt;/P&gt;</description>
    <pubDate>Thu, 26 Dec 2024 02:32:12 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2024-12-26T02:32:12Z</dc:date>
    <item>
      <title>S32K3 CAN communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019343#M44585</link>
      <description>&lt;P&gt;Hi NXP's team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;i have some problems,&amp;nbsp;I attach the source code below&lt;/P&gt;&lt;P&gt;*My Target&lt;/P&gt;&lt;P&gt;-CAN communication between S32K344 and CAN tool based&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;/P&gt;&lt;P&gt;*My hardware and Software&lt;/P&gt;&lt;P&gt;-S32K3x4EVB T172/orQ172 i'm not sure,&amp;nbsp; &amp;nbsp;S32DS 3.5,&amp;nbsp; RTD 5.0.0&lt;/P&gt;&lt;P&gt;-I connected CANH, CANL, CAN_GND each togeter between Board and CAN Tool, but no date was be traced&lt;/P&gt;&lt;P&gt;*Can you check if they work on your side, and point out my mistakes?&lt;/P&gt;</description>
      <pubDate>Wed, 25 Dec 2024 10:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019343#M44585</guid>
      <dc:creator>Voledi</dc:creator>
      <dc:date>2024-12-25T10:44:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 CAN communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019443#M44593</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;Voledi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;S32K3X4-T172 and S32K3X4-Q172 are different, and the CAN transceiver are different.&lt;/P&gt;
&lt;P&gt;This demo is based on S32K3X4-Q172, and the transceiver used is TJA1153.&lt;/P&gt;
&lt;P&gt;And this demo is based on S32 DS V3.4+ RTD 2.0.0, which is not compatible with the version you are using.&lt;/P&gt;
&lt;P&gt;The attached is a routine based on &lt;STRONG&gt;S32K311&lt;/STRONG&gt;, you can refer to it, the version is consistent with what you are currently using.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Dec 2024 02:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019443#M44593</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-12-26T02:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 CAN communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019475#M44595</link>
      <description>&lt;P&gt;Can you identify the exact type of board, I'm confused about this&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Voledi_0-1735182782568.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/317323iA4A056D28AB90ECC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Voledi_0-1735182782568.jpeg" alt="Voledi_0-1735182782568.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Voledi_0-1735182782568.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;MCU:&amp;nbsp;&lt;SPAN&gt;P32K344EHVPBS0P55A&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Dec 2024 03:13:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019475#M44595</guid>
      <dc:creator>Voledi</dc:creator>
      <dc:date>2024-12-26T03:13:41Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 CAN communication</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019545#M44597</link>
      <description>&lt;P&gt;Hi@&lt;SPAN&gt;Voledi&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;According to the information in the picture, the transceiver here should be TJA1153, so there is no problem if you refer to this link, but this is based on S32 DS V3.4 + RTD 2.0.0.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test-S32DS3-4/ta-p/1536225&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Dec 2024 06:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-CAN-communication/m-p/2019545#M44597</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-12-26T06:20:23Z</dc:date>
    </item>
  </channel>
</rss>