<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 witch UTEST address can customer use？ in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/2019273#M44584</link>
    <description>&lt;P&gt;&lt;SPAN&gt;The UTEST area(0x1B00_0048-0x1B00_007F) is&amp;nbsp;&lt;STRONG&gt;programmable&lt;/STRONG&gt;&amp;nbsp;by the Application. Hence the description in HSE_b RM is incorrect and it will be updated in the upcoming version v2.4.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;According to the latest feedback from HSE team, they speculate that another&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;HSE write&amp;nbsp;operation&amp;nbsp;was executing when APP was programming data at&amp;nbsp;0x1b00_0048 - 0x1b00_004f simultaneously would cause this issue.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So the customer can try to add below check and&amp;nbsp;also wait for HSE_STATUS_INIT_OK, before writing into the UTEST area.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 141. Status Bits on HSE GPR Register 3 (0x4039C028).png" style="width: 835px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/317260iB0F758B82CD277DE/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 141. Status Bits on HSE GPR Register 3 (0x4039C028).png" alt="Table 141. Status Bits on HSE GPR Register 3 (0x4039C028).png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 25 Dec 2024 07:47:05 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-12-25T07:47:05Z</dc:date>
    <item>
      <title>S32K3 witch UTEST address can customer use？</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/1976079#M42218</link>
      <description>&lt;P&gt;我们发现S32K3&amp;nbsp;&amp;nbsp;S32K3xx_DCF_clients.xlsx文件里描述的“Reserved for customer/application usage”的区域是有问题的。我们测试的时候，写入数据到0x1B000050~0X1B000058，程序可正常运行。然而，我们测试将同样的数据写入到0x1B000048~0x1B00004F，程序工作异常，出现周期复位情况，经过测试，需要在时钟初始化前增加几十毫秒的延时才能正常运行。对此，我们认为，0x1B000048~0x1B00004F写入数据会对S32K3的运行有未知的影响。那么UTEST区域有哪些地址是我们用户可以随意使用的呢？您能给一些建议吗？谢谢！&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 12:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/1976079#M42218</guid>
      <dc:creator>zhengjianfei1</dc:creator>
      <dc:date>2024-10-17T12:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 witch UTEST address can customer use？</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/1976782#M42262</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;Table 135. UTEST Device configuration&lt;/EM&gt;&lt;/STRONG&gt; of &lt;STRONG&gt;&lt;EM&gt;RM758223-HSE-B Firmware Reference Manual - V2.3(2.3).pdf&lt;/EM&gt;&lt;/STRONG&gt; mentions: &lt;STRONG&gt;0x1B000048&lt;/STRONG&gt; 8 bytes &lt;U&gt;Used by HSE. Must not be programmed by application&lt;/U&gt;.&lt;BR /&gt;Sorry, the information in &lt;EM&gt;&lt;STRONG&gt;S32K3xx_DCF_clients.xlsx&lt;/STRONG&gt;&lt;/EM&gt; conflicts with &lt;STRONG&gt;&lt;EM&gt;RM758223-HSE-B Firmware Reference Manual - V2.3(2.3).pdf&lt;/EM&gt;&lt;/STRONG&gt;. I need to consult it with our AE team and will update as soon as I have their feedback.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 07:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/1976782#M42262</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-10-18T07:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 witch UTEST address can customer use？</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/1976856#M42266</link>
      <description>谢谢您Robin，另外能否也帮忙问问AE Team写入0X1B000048~1B00004F后，会有什么影响或风险吗？目前已经有多个产品已经写入了这个地址了。</description>
      <pubDate>Fri, 18 Oct 2024 08:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/1976856#M42266</guid>
      <dc:creator>zhengjianfei1</dc:creator>
      <dc:date>2024-10-18T08:22:38Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 witch UTEST address can customer use？</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/2019273#M44584</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The UTEST area(0x1B00_0048-0x1B00_007F) is&amp;nbsp;&lt;STRONG&gt;programmable&lt;/STRONG&gt;&amp;nbsp;by the Application. Hence the description in HSE_b RM is incorrect and it will be updated in the upcoming version v2.4.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;According to the latest feedback from HSE team, they speculate that another&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;HSE write&amp;nbsp;operation&amp;nbsp;was executing when APP was programming data at&amp;nbsp;0x1b00_0048 - 0x1b00_004f simultaneously would cause this issue.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;So the customer can try to add below check and&amp;nbsp;also wait for HSE_STATUS_INIT_OK, before writing into the UTEST area.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Table 141. Status Bits on HSE GPR Register 3 (0x4039C028).png" style="width: 835px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/317260iB0F758B82CD277DE/image-size/large?v=v2&amp;amp;px=999" role="button" title="Table 141. Status Bits on HSE GPR Register 3 (0x4039C028).png" alt="Table 141. Status Bits on HSE GPR Register 3 (0x4039C028).png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Dec 2024 07:47:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-witch-UTEST-address-can-customer-use/m-p/2019273#M44584</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-12-25T07:47:05Z</dc:date>
    </item>
  </channel>
</rss>