<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K148 write and read P_FLASH</title>
    <link>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898572#M4438</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks ,I've worked it out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Apr 2019 01:19:55 GMT</pubDate>
    <dc:creator>347996379</dc:creator>
    <dc:date>2019-04-18T01:19:55Z</dc:date>
    <item>
      <title>S32K148 write and read P_FLASH</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898570#M4436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;I've programed P_FLASH,but reading P-FLASH failed,&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;I'm not sure which funtion reads P_FLASH?&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;• status_t &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ReadOnce &lt;/SPAN&gt;&lt;SPAN class=""&gt;(const &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;flash_ssd_config_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pSSDConfig, uint8_t recordIndex, uint8_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;p &lt;/SPAN&gt;&lt;SPAN class=""&gt;-&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;DataArray)&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Flash read once.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;• status_t &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ProgramOnce &lt;/SPAN&gt;&lt;SPAN class=""&gt;(const &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;flash_ssd_config_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pSSDConfig, uint8_t recordIndex, const&lt;BR /&gt;uint8_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pDataArray)&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Flash program once.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;• status_t &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_Program &lt;/SPAN&gt;&lt;SPAN class=""&gt;(const &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;flash_ssd_config_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pSSDConfig, uint32_t dest, uint32_t size, const&lt;BR /&gt;uint8_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pData)&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;Flash program.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;• status_t &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ProgramCheck &lt;/SPAN&gt;&lt;SPAN class=""&gt;(const &lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;flash_ssd_config_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pSSDConfig, uint32_t dest, uint32_t size,&lt;BR /&gt;const uint8_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pExpectedData, uint32_t &lt;/SPAN&gt;&lt;SPAN class=""&gt;∗&lt;/SPAN&gt;&lt;SPAN class=""&gt;pFailAddr, uint8_t marginLevel)&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Flash program check&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;or more?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 02:24:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898570#M4436</guid>
      <dc:creator>347996379</dc:creator>
      <dc:date>2019-04-17T02:24:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 write and read P_FLASH</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898571#M4437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you want to just simply read the content of flash, use pointers. There's no such general function.&lt;/P&gt;&lt;P&gt;Mentioned functions &lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ReadOnce &lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt; and &lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ProgramCheck &lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;are used for something different:&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ReadOnce&lt;/SPAN&gt; - it is used for reading of Program Once field in IFR section of PFlash. It can't be used for normal PFlash. &lt;/P&gt;&lt;P&gt;&lt;SPAN class="" style="color: #0000ff;"&gt;FLASH_DRV_ProgramCheck &lt;/SPAN&gt;- this command tests a previously programmed program flash or data flash longword to see if it reads correctly at the specified margin level.&amp;nbsp; &lt;SPAN class="" style="color: #0000ff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 10:46:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898571#M4437</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2019-04-17T10:46:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K148 write and read P_FLASH</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898572#M4438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks ,I've worked it out.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 01:19:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/898572#M4438</guid>
      <dc:creator>347996379</dc:creator>
      <dc:date>2019-04-18T01:19:55Z</dc:date>
    </item>
    <item>
      <title>S32K144 write and read P_FLASH</title>
      <link>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/1751619#M28381</link>
      <description>&lt;P&gt;hello can you pllease guide how to read data from flash (NVRAM) base address using pointer in s32k144evb-q100.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Nov 2023 05:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K148-write-and-read-P-FLASH/m-p/1751619#M28381</guid>
      <dc:creator>gopichauhan</dc:creator>
      <dc:date>2023-11-03T05:51:29Z</dc:date>
    </item>
  </channel>
</rss>