<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K344-Application debug authorization mode</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2015877#M44367</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218611"&gt;@Simon-Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"Table 194. Feature configuration in CUST_DEL Device Life Cycle" shows what should be configured in CUST_DEL life cycle. It does not say that these features take effect in CUST_DEL life cycle.&lt;/P&gt;
&lt;P&gt;Debuging of HSE core is not allowed for users at all. &lt;BR /&gt;Application debug port is open in CUST_DEL life cycle. After advancing to OEM_PROD or to IN_FIELD, it is mandatory to use ADKP (password or key).&lt;/P&gt;
&lt;P&gt;If you don't use HSE, you can follow this article:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you use HSE, the ADKP configuration should be done by HSE services. You can find an example in this package:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;BR /&gt;The example is:&lt;BR /&gt;c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Device_Configuration\S32K344_CQC_DEMO\&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Wed, 18 Dec 2024 06:59:26 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-12-18T06:59:26Z</dc:date>
    <item>
      <title>S32K344-Application debug authorization mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2014871#M44309</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I see in RM that in the table [Feature configuration in CUST_DEL Device Life Cycle] there are settings as shown in the figure below. When modifying the debugging mode through HSE, is the debugging of the Application software?&lt;BR /&gt;The default state is Password-based approach, but I can debug directly using S32DS without using HSE, without a password.&lt;BR /&gt;Or does the debugging here refer to debugging HSE?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 03:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2014871#M44309</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-12-17T03:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-Application debug authorization mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2015877#M44367</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218611"&gt;@Simon-Liu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"Table 194. Feature configuration in CUST_DEL Device Life Cycle" shows what should be configured in CUST_DEL life cycle. It does not say that these features take effect in CUST_DEL life cycle.&lt;/P&gt;
&lt;P&gt;Debuging of HSE core is not allowed for users at all. &lt;BR /&gt;Application debug port is open in CUST_DEL life cycle. After advancing to OEM_PROD or to IN_FIELD, it is mandatory to use ADKP (password or key).&lt;/P&gt;
&lt;P&gt;If you don't use HSE, you can follow this article:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Restrict-the-debug-access-with-a-password-when-HSE-is-not/ta-p/1735073&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;If you use HSE, the ADKP configuration should be done by HSE services. You can find an example in this package:&lt;BR /&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;BR /&gt;The example is:&lt;BR /&gt;c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Device_Configuration\S32K344_CQC_DEMO\&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 06:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2015877#M44367</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-12-18T06:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344-Application debug authorization mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2015880#M44370</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37795"&gt;@lukaszadrapa&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;BR /&gt;I understand that whether a password is required for debugging is related to the life cycle.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BestRegards,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 07:04:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-Application-debug-authorization-mode/m-p/2015880#M44370</guid>
      <dc:creator>Simon-Liu</dc:creator>
      <dc:date>2024-12-18T07:04:31Z</dc:date>
    </item>
  </channel>
</rss>