<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3 FLASH write in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2013485#M44228</link>
    <description>&lt;P&gt;Hi, everyone&lt;/P&gt;&lt;P&gt;I am using the first core of the S32K358 chip to program, I want to put the BOOTLOADER program in the memory of PFLASH0, and then put the APP program in the memory of PFLASH1, can the APP run properly?&lt;/P&gt;</description>
    <pubDate>Fri, 13 Dec 2024 09:04:24 GMT</pubDate>
    <dc:creator>DouDou1</dc:creator>
    <dc:date>2024-12-13T09:04:24Z</dc:date>
    <item>
      <title>S32K3 FLASH write</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2013485#M44228</link>
      <description>&lt;P&gt;Hi, everyone&lt;/P&gt;&lt;P&gt;I am using the first core of the S32K358 chip to program, I want to put the BOOTLOADER program in the memory of PFLASH0, and then put the APP program in the memory of PFLASH1, can the APP run properly?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 09:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2013485#M44228</guid>
      <dc:creator>DouDou1</dc:creator>
      <dc:date>2024-12-13T09:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 FLASH write</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2015064#M44319</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230579"&gt;@DouDou1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, there's no problem with this setup. There are four code flash blocks and read-while-write is supported between these blocks.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 08:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2015064#M44319</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-12-17T08:43:21Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 FLASH write</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2015759#M44356</link>
      <description>&lt;P&gt;Hi,@lukaszadrapa,&lt;BR /&gt;Thank you for your reply, I want to know if the first core of the S32K358 chip can read-while-write all four code?&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 03:33:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2015759#M44356</guid>
      <dc:creator>DouDou1</dc:creator>
      <dc:date>2024-12-18T03:33:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 FLASH write</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2015893#M44372</link>
      <description>&lt;P&gt;It doesn't matter which master accesses a flash block.&lt;/P&gt;
&lt;P&gt;There's simple rule - if a block is being erased or programmed, it's now allowed to access this block. Only other blocks can be accessed at that time.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 07:14:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2015893#M44372</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-12-18T07:14:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 FLASH write</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2016742#M44401</link>
      <description>Thank you for your reply.&lt;BR /&gt;</description>
      <pubDate>Thu, 19 Dec 2024 02:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-FLASH-write/m-p/2016742#M44401</guid>
      <dc:creator>DouDou1</dc:creator>
      <dc:date>2024-12-19T02:26:21Z</dc:date>
    </item>
  </channel>
</rss>