<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32DS IDE installation  and development package installation for s32k3xx in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2011330#M44109</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN&gt;&amp;nbsp; After S32DS 3.5 IDE installation, I opened an example Flex CAN project&amp;nbsp; from RTD&amp;nbsp; s32kxx and built it. I got the errors as are below,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In file included from ../board/Siul2_Port_Ip_Cfg.c:42:&lt;BR /&gt;../board/Siul2_Port_Ip_Cfg.h:46:10: fatal error: Siul2_Port_Ip_Types.h: No such file or directory&lt;BR /&gt;46 | #include "Siul2_Port_Ip_Types.h"&lt;/P&gt;&lt;P&gt;C:/Users/karme/workspaceS32DS.3.5/FlexCAN_Ip_Example_S32K344/RTD/include/CanIf.h:52:10: fatal error: CanIf_Cfg.h: No such file or directory&lt;BR /&gt;52 | #include "CanIf_Cfg.h"&lt;BR /&gt;| ^~~~~~~~~~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;make: *** [RTD/src/subdir.mk:38: RTD/src/CanIf.o] Error 1&lt;BR /&gt;In file included from ../RTD/src/Can_43_FLEXCAN.c:104:&lt;BR /&gt;C:/Users/karme/workspaceS32DS.3.5/FlexCAN_Ip_Example_S32K344/RTD/include/Can_43_FLEXCAN.h:110:10: fatal error: Soc_Ips.h: No such file or directory&lt;BR /&gt;110 | #include "Soc_Ips.h"&lt;BR /&gt;| ^~~~~~~~~~~&lt;/P&gt;&lt;P&gt;How to fix these mistakes I need your help with the S32DS IDE, S32K3xx development package, and RTD installation since I believe there may have been errors in the package and IDE installation time.&lt;BR /&gt;There are drivers for the boot loader, CAN, UDS, and FLASHING S32K342 in the RTD or S32K3xx development packages.&lt;/P&gt;</description>
    <pubDate>Tue, 10 Dec 2024 21:01:34 GMT</pubDate>
    <dc:creator>karmegancjk</dc:creator>
    <dc:date>2024-12-10T21:01:34Z</dc:date>
    <item>
      <title>S32K3xx MCU programmer and debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2010721#M44072</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Kindly suggest cost effective S32K3xx cortex m7&amp;nbsp; programmer and debugger&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Karmegan C&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 05:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2010721#M44072</guid>
      <dc:creator>karmegancjk</dc:creator>
      <dc:date>2024-12-10T05:47:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx MCU programmer and debugger</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2010829#M44075</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There is wide variety of devices you can use.&lt;/P&gt;
&lt;P&gt;It depends on how serious you will go with your development.&lt;/P&gt;
&lt;P&gt;Very basic - is embedded open SDA - free on the evaluation boards.&lt;/P&gt;
&lt;P&gt;basic - PE micro&lt;/P&gt;
&lt;P&gt;advanced - iSystem, GHS probe&lt;/P&gt;
&lt;P&gt;Pro - Lauterbach&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 08:11:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2010829#M44075</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-12-10T08:11:18Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS IDE installation  and development package installation for s32k3xx</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2011330#M44109</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &lt;SPAN&gt;&amp;nbsp; After S32DS 3.5 IDE installation, I opened an example Flex CAN project&amp;nbsp; from RTD&amp;nbsp; s32kxx and built it. I got the errors as are below,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;In file included from ../board/Siul2_Port_Ip_Cfg.c:42:&lt;BR /&gt;../board/Siul2_Port_Ip_Cfg.h:46:10: fatal error: Siul2_Port_Ip_Types.h: No such file or directory&lt;BR /&gt;46 | #include "Siul2_Port_Ip_Types.h"&lt;/P&gt;&lt;P&gt;C:/Users/karme/workspaceS32DS.3.5/FlexCAN_Ip_Example_S32K344/RTD/include/CanIf.h:52:10: fatal error: CanIf_Cfg.h: No such file or directory&lt;BR /&gt;52 | #include "CanIf_Cfg.h"&lt;BR /&gt;| ^~~~~~~~~~~~~&lt;BR /&gt;compilation terminated.&lt;BR /&gt;make: *** [RTD/src/subdir.mk:38: RTD/src/CanIf.o] Error 1&lt;BR /&gt;In file included from ../RTD/src/Can_43_FLEXCAN.c:104:&lt;BR /&gt;C:/Users/karme/workspaceS32DS.3.5/FlexCAN_Ip_Example_S32K344/RTD/include/Can_43_FLEXCAN.h:110:10: fatal error: Soc_Ips.h: No such file or directory&lt;BR /&gt;110 | #include "Soc_Ips.h"&lt;BR /&gt;| ^~~~~~~~~~~&lt;/P&gt;&lt;P&gt;How to fix these mistakes I need your help with the S32DS IDE, S32K3xx development package, and RTD installation since I believe there may have been errors in the package and IDE installation time.&lt;BR /&gt;There are drivers for the boot loader, CAN, UDS, and FLASHING S32K342 in the RTD or S32K3xx development packages.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 21:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2011330#M44109</guid>
      <dc:creator>karmegancjk</dc:creator>
      <dc:date>2024-12-10T21:01:34Z</dc:date>
    </item>
    <item>
      <title>Re: S32DS IDE installation  and development package installation for s32k3xx</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2011782#M44142</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Sorry, this is different topic.&lt;/P&gt;
&lt;P&gt;I am not able to help here. Always respect the release notes of RTD packages, otherwise the packages will not be compatible.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 11 Dec 2024 08:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-MCU-programmer-and-debugger/m-p/2011782#M44142</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-12-11T08:31:49Z</dc:date>
    </item>
  </channel>
</rss>