<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: CAN HighLevel API - No signals on osci</title>
    <link>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2011116#M44099</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;seems you started CanController_0 which is configured for loopback mode in setting, so you get no signals on module pins (PTA6/7 or PTB0/1).&amp;nbsp;CanController_1 is not set for loopback mode, but it is not started at all, so no transfer can be seen on its pins (PTC8/9).&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Tue, 10 Dec 2024 14:00:21 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-12-10T14:00:21Z</dc:date>
    <item>
      <title>CAN HighLevel API - No signals on osci</title>
      <link>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2010896#M44085</link>
      <description>&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope you are doing fine today. I have a question about CAN. So I tried the CAN example with low level API, which is working fine, even if I reroute the PINS from PTA6/7 -&amp;gt; PTB0/1. I can see all the send signals on osci. For sure PTB0/1 are without a CAN transceiver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;But If I try now the CAN high level API example, with configured PINS,PORT, CAN_43_FLEXCAN,..in S32DS. Code is generated without any error and project is also compiling and linking. But I cannot see any signals on the osci. Neither on PTA6/7 nor on PTB0/1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the attachement you can finde the example of the High Level API.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any help in advance!&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 09:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2010896#M44085</guid>
      <dc:creator>nxp_user001123</dc:creator>
      <dc:date>2024-12-10T09:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: CAN HighLevel API - No signals on osci</title>
      <link>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2011116#M44099</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;seems you started CanController_0 which is configured for loopback mode in setting, so you get no signals on module pins (PTA6/7 or PTB0/1).&amp;nbsp;CanController_1 is not set for loopback mode, but it is not started at all, so no transfer can be seen on its pins (PTC8/9).&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 10 Dec 2024 14:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2011116#M44099</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-12-10T14:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: CAN HighLevel API - No signals on osci</title>
      <link>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2014183#M44273</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Loopback was one of the issues, the other was to connect another CAN-node on the bus to get the example working.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Dec 2024 06:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-HighLevel-API-No-signals-on-osci/m-p/2014183#M44273</guid>
      <dc:creator>nxp_user001123</dc:creator>
      <dc:date>2024-12-16T06:56:28Z</dc:date>
    </item>
  </channel>
</rss>