<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K ADC + DMA + PDB trigger</title>
    <link>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896893#M4408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felix, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right. For ADC trigger source options you only have the following signals ADC0_SC1A[COCO], ADC0_SC1B[COCO], ADC1_SC1A[COCO], and ADC1_SC1B[COCO].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Apr 2019 17:14:56 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2019-04-30T17:14:56Z</dc:date>
    <item>
      <title>S32K ADC + DMA + PDB trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896889#M4404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i same problem here, in chapter 44.3.1 (ref. manual 8, 06/2018) i would like to know the PDB trigger sources. it says &lt;BR /&gt;"Refer to chip configuration details for the actual PDB input trigger"&lt;BR /&gt;&lt;BR /&gt;but i cant find it. in the attached excel files are only the trigmux trigger which dont fit into 4 bit.&lt;BR /&gt;&lt;BR /&gt;thanks!&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 07:37:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896889#M4404</guid>
      <dc:creator>felix_niessen</dc:creator>
      <dc:date>2019-04-09T07:37:16Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC + DMA + PDB trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896890#M4405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To explain it a bit more, i would like to have the ADC sample one channel&amp;nbsp;continuous until i stop it. the samples should be stored by DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;DMA part is working, but i need to have the ADC COCO triggering back the PDB so it starts the next conversion.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for now i can sample the four&amp;nbsp;SC1 inputs but then i need to restart the PDB manual (DMA interrupt or Loop).&lt;BR /&gt;&lt;BR /&gt;thanks!&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 13:27:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896890#M4405</guid>
      <dc:creator>felix_niessen</dc:creator>
      <dc:date>2019-04-15T13:27:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC + DMA + PDB trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896891#M4406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felix,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In section 44.1.1.2 of the reference manual says: "&lt;EM&gt;On this device, the PDB trigger source selection is implemented through the TRGMUX module. &lt;STRONG&gt;For each PDB unit, there is only one trigger input from TRGMUX,&lt;/STRONG&gt; but it supports different trigger sources. The internal trigger mux inside PDB is not used anymore.&lt;/EM&gt;"&lt;/P&gt;&lt;P&gt;So, from the Trigger input source select, the only option you have is &lt;STRONG&gt;0000 Trigger-In 0 selected&lt;/STRONG&gt;. All the other options are now reserved.&lt;/P&gt;&lt;P&gt;From the RM Figure 19-2, you can see that you have the following Trigger Source options: ADC0_SC1A[COCO] in30, ADC0_SC1B[COCO] in31, ADC1_SC1A[COCO]in32, and ADC1_SC1B[COCO] in33. For example, If you want to target module PDB0_trigger_in0 with ADC0_SC1A[COCO] then in the field SEL0 of the register&amp;nbsp;TRGMUX PDB0 you need to put the 30.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79126i9DE451B54D254EDF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 21:47:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896891#M4406</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-04-15T21:47:31Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC + DMA + PDB trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896892#M4407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, yes this answers my question. Thanks! Will try it tomorrow.&lt;/P&gt;&lt;P&gt;Am i right that there is no direct way to have the adc trigger it self? Like a continous conversion of one channel?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Felix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2019 15:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896892#M4407</guid>
      <dc:creator>felix_niessen</dc:creator>
      <dc:date>2019-04-29T15:22:17Z</dc:date>
    </item>
    <item>
      <title>Re: S32K ADC + DMA + PDB trigger</title>
      <link>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896893#M4408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Felix, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right. For ADC trigger source options you only have the following signals ADC0_SC1A[COCO], ADC0_SC1B[COCO], ADC1_SC1A[COCO], and ADC1_SC1B[COCO].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Apr 2019 17:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-ADC-DMA-PDB-trigger/m-p/896893#M4408</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2019-04-30T17:14:56Z</dc:date>
    </item>
  </channel>
</rss>