<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K3 Lin Slave Mode Issue in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-Lin-Slave-Mode-Issue/m-p/2008948#M43968</link>
    <description>&lt;P&gt;Dear S32K3 Team,&lt;/P&gt;&lt;P&gt;I hope this message finds you well.&lt;BR /&gt;I am currently facing issues while attempting communication using LIN-LPUART on the S32K311 and would like to request your assistance. Below, I have outlined the issues I am encountering and would greatly appreciate any solutions or guidance you can provide.&lt;/P&gt;&lt;P&gt;1. In master mode, when transmitting LIN data in the response-rx format, Canoe detects an "Incorrect sync delimiter length" error.&lt;BR /&gt;1.1.&amp;nbsp; Despite this, Canoe sends a response, but the LIN IRQ handler detects a framing error, preventing the correct response from being transmitted.&lt;/P&gt;&lt;P&gt;2. I require an example for the slave mode. (RTD Version: SW32K3_RTD_R21-11_3.0.0_P07)&lt;BR /&gt;2.1.&amp;nbsp; After initializing in slave mode and running the program, I observed that the waveform of the LIN bus matches the LPUART-RX pin when a message is sent from Canoe. However, no interrupt occurs, and the IRQ handler is not triggered.&lt;/P&gt;&lt;P&gt;I sincerely hope to receive guidance or solutions regarding these issues.&lt;BR /&gt;Thank you very much for your time and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
    <pubDate>Fri, 06 Dec 2024 08:18:29 GMT</pubDate>
    <dc:creator>NewbieNerd</dc:creator>
    <dc:date>2024-12-06T08:18:29Z</dc:date>
    <item>
      <title>S32K3 Lin Slave Mode Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Lin-Slave-Mode-Issue/m-p/2008948#M43968</link>
      <description>&lt;P&gt;Dear S32K3 Team,&lt;/P&gt;&lt;P&gt;I hope this message finds you well.&lt;BR /&gt;I am currently facing issues while attempting communication using LIN-LPUART on the S32K311 and would like to request your assistance. Below, I have outlined the issues I am encountering and would greatly appreciate any solutions or guidance you can provide.&lt;/P&gt;&lt;P&gt;1. In master mode, when transmitting LIN data in the response-rx format, Canoe detects an "Incorrect sync delimiter length" error.&lt;BR /&gt;1.1.&amp;nbsp; Despite this, Canoe sends a response, but the LIN IRQ handler detects a framing error, preventing the correct response from being transmitted.&lt;/P&gt;&lt;P&gt;2. I require an example for the slave mode. (RTD Version: SW32K3_RTD_R21-11_3.0.0_P07)&lt;BR /&gt;2.1.&amp;nbsp; After initializing in slave mode and running the program, I observed that the waveform of the LIN bus matches the LPUART-RX pin when a message is sent from Canoe. However, no interrupt occurs, and the IRQ handler is not triggered.&lt;/P&gt;&lt;P&gt;I sincerely hope to receive guidance or solutions regarding these issues.&lt;BR /&gt;Thank you very much for your time and assistance.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 08:18:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Lin-Slave-Mode-Issue/m-p/2008948#M43968</guid>
      <dc:creator>NewbieNerd</dc:creator>
      <dc:date>2024-12-06T08:18:29Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Lin Slave Mode Issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Lin-Slave-Mode-Issue/m-p/2009868#M44017</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1) this can point to bit timing issue. Be sure bitrate is set similarly. You can measure geenrated signal on TX/RX if it as expected.&lt;/P&gt;
&lt;P&gt;2)&amp;nbsp;&lt;SPAN&gt;here are two RTD demos you can refer to, where LPUART is used as LIN Slave&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;-&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;"Lin_Ip_FrameTransfer_S32K344"...&amp;nbsp; simple application which shows a communication between a Lin Master and a Lin Slave of both Lpuart Ip and Flexio Ip&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;BR clear="none" /&gt;&lt;SPAN&gt;- "Lin_Slave_S32K344_Example_DS" ... LINStack example demonstrating the LIN communication between S32K344 Slave and other board Master using unconditional frames.&lt;BR /&gt;There is no direct example for S32K311, but you can reuse existed one to create new. For slave mode be sure&amp;nbsp;module interrupt is properly enabled and Auto-detect baudrate feature&amp;nbsp;is properly implemented, as shown in the example and described in&amp;nbsp;&amp;nbsp;the chapter&amp;nbsp;&lt;STRONG&gt;&lt;EM&gt;3.6.5 Auto-detect baudrate feature&lt;/EM&gt;&lt;/STRONG&gt;&amp;nbsp;of&amp;nbsp;&lt;EM&gt;RTD_LIN_43_LPUART_FLEXIO_UM.pdf&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 08:55:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Lin-Slave-Mode-Issue/m-p/2009868#M44017</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-12-09T08:55:53Z</dc:date>
    </item>
  </channel>
</rss>