<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPUART FIFO in S32K</title>
    <link>https://community.nxp.com/t5/S32K/LPUART-FIFO/m-p/895619#M4372</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the S32K146 and I'm trying to set up the LPUART to work with a FIFO buffer of 64 or 128 bytes using a polling method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm setting TXFE and RXFE of the FIFO register to enable Rx and Tx FIFO's (LPUART1-&amp;gt;FIFO = 0x00000088), but TXFIFOSIZE and RXFIFOSIZE on the FIFO register say their read only, so how would I set the FIFO buffer depth?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set RXWATER to be 3 as this is the maximum value, but then RDRF on the STAT register is set when only 4 words are received. Does this mean that the maximum FIFO size is 4 words? As in the manual it says its up to 256 words?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried reading the received data when RXCOUNT has reached a certain number of bytes, but it again only seems to work for a maximum of 4 words?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 May 2019 12:02:19 GMT</pubDate>
    <dc:creator>jay_montague</dc:creator>
    <dc:date>2019-05-15T12:02:19Z</dc:date>
    <item>
      <title>LPUART FIFO</title>
      <link>https://community.nxp.com/t5/S32K/LPUART-FIFO/m-p/895619#M4372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the S32K146 and I'm trying to set up the LPUART to work with a FIFO buffer of 64 or 128 bytes using a polling method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm setting TXFE and RXFE of the FIFO register to enable Rx and Tx FIFO's (LPUART1-&amp;gt;FIFO = 0x00000088), but TXFIFOSIZE and RXFIFOSIZE on the FIFO register say their read only, so how would I set the FIFO buffer depth?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set RXWATER to be 3 as this is the maximum value, but then RDRF on the STAT register is set when only 4 words are received. Does this mean that the maximum FIFO size is 4 words? As in the manual it says its up to 256 words?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried reading the received data when RXCOUNT has reached a certain number of bytes, but it again only seems to work for a maximum of 4 words?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jay&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 May 2019 12:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/LPUART-FIFO/m-p/895619#M4372</guid>
      <dc:creator>jay_montague</dc:creator>
      <dc:date>2019-05-15T12:02:19Z</dc:date>
    </item>
  </channel>
</rss>