<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 FlashDriver can not use</title>
    <link>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2003491#M43712</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P class="lia-align-justify"&gt;I use the file (S32K358_FLASH_TEST) to generate the.s19 file of FlashDriver, and then test it in the file (S32K358_TCU_FlashDriver_TEST). When I test, Run C40Status = ((C40_Ip_Init)(Function_TABLE[0]))(&amp;amp;C40_Ip_InitCfg). When this statement, the program will jump to the error interrupt void HardFault_Handler(void), I have tried many methods, but it does not work, what is the reason for this?&lt;/P&gt;&lt;P class="lia-align-justify"&gt;I refer to this method &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-How-to-make-Flash-Driver-image/ta-p/1630873" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-How-to-make-Flash-Driver-image/ta-p/1630873&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 28 Nov 2024 07:50:17 GMT</pubDate>
    <dc:creator>DouDou1</dc:creator>
    <dc:date>2024-11-28T07:50:17Z</dc:date>
    <item>
      <title>FlashDriver can not use</title>
      <link>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2003491#M43712</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P class="lia-align-justify"&gt;I use the file (S32K358_FLASH_TEST) to generate the.s19 file of FlashDriver, and then test it in the file (S32K358_TCU_FlashDriver_TEST). When I test, Run C40Status = ((C40_Ip_Init)(Function_TABLE[0]))(&amp;amp;C40_Ip_InitCfg). When this statement, the program will jump to the error interrupt void HardFault_Handler(void), I have tried many methods, but it does not work, what is the reason for this?&lt;/P&gt;&lt;P class="lia-align-justify"&gt;I refer to this method &lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-How-to-make-Flash-Driver-image/ta-p/1630873" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-How-to-make-Flash-Driver-image/ta-p/1630873&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Nov 2024 07:50:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2003491#M43712</guid>
      <dc:creator>DouDou1</dc:creator>
      <dc:date>2024-11-28T07:50:17Z</dc:date>
    </item>
    <item>
      <title>Re: FlashDriver can not use</title>
      <link>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2005116#M43798</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230579"&gt;@DouDou1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;did you try to step the code to see where it fails exactly? Are all functions referenced in the init function also forced to that specific segment?&lt;/P&gt;
&lt;P&gt;I would rather use flash drivers from HSE examples:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=S32K3_HSE_DemoExamples&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Install the package and then you will find the drivers at path like this:&lt;/P&gt;
&lt;P&gt;c:\NXP\S32K3_HSE_DemoExamples_1_0_0\S32K3_HSE_DemoExamples\Asymmetric Algorithms\S32K344_Hse_Ecc_Example\drivers\flash\&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 11:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2005116#M43798</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-12-02T11:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: FlashDriver can not use</title>
      <link>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2005672#M43825</link>
      <description>Hi,@lukaszadrapa&lt;BR /&gt;Thanks for you reply, I try to step the code in this file(S32K358_TCU_FlashDriver_TEST). When I test, Run C40Status = ((C40_Ip_Init)(Function_TABLE[0]))(&amp;amp;C40_Ip_InitCfg),the program will jump to the error interrupt void HardFault_Handler(void).&lt;BR /&gt;And I checked that all functions referenced in the init function also were forced to that specific segment.</description>
      <pubDate>Tue, 03 Dec 2024 05:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlashDriver-can-not-use/m-p/2005672#M43825</guid>
      <dc:creator>DouDou1</dc:creator>
      <dc:date>2024-12-03T05:21:46Z</dc:date>
    </item>
  </channel>
</rss>