<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRTD drivers for MC33774A</title>
    <link>https://community.nxp.com/t5/S32K/RTD-drivers-for-MC33774A/m-p/1999711#M43517</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using the MC33774A AFE in our non-AUTOSAR project. Since there is no non-AUTOSAR MC33774A driver available, we are using the AUTOSAR driver. In the example code, I noticed additional AUTOSAR drivers, such as GPT, Direct SPI, and BMS_Common, which are required for BCC_774A functionality. My question is: is it acceptable to use all these AUTOSAR drivers in a non-AUTOSAR project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mohana G V&lt;/P&gt;</description>
    <pubDate>Fri, 22 Nov 2024 04:21:36 GMT</pubDate>
    <dc:creator>mohanagv</dc:creator>
    <dc:date>2024-11-22T04:21:36Z</dc:date>
    <item>
      <title>RTD drivers for MC33774A</title>
      <link>https://community.nxp.com/t5/S32K/RTD-drivers-for-MC33774A/m-p/1999711#M43517</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using the MC33774A AFE in our non-AUTOSAR project. Since there is no non-AUTOSAR MC33774A driver available, we are using the AUTOSAR driver. In the example code, I noticed additional AUTOSAR drivers, such as GPT, Direct SPI, and BMS_Common, which are required for BCC_774A functionality. My question is: is it acceptable to use all these AUTOSAR drivers in a non-AUTOSAR project?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mohana G V&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 04:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-drivers-for-MC33774A/m-p/1999711#M43517</guid>
      <dc:creator>mohanagv</dc:creator>
      <dc:date>2024-11-22T04:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: RTD drivers for MC33774A</title>
      <link>https://community.nxp.com/t5/S32K/RTD-drivers-for-MC33774A/m-p/2000341#M43564</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/239661"&gt;@mohanagv&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It is fine to use both AUTOSAR and non-AUTOSAR drivers in the project, but there are some limitations when mixing them:&lt;/P&gt;
&lt;P&gt;1. It is forbidden to use the same hardware instance in HLD and LLD (E.g. if SPI1 is used in HLD context, it cannot be used also through IPL)&lt;/P&gt;
&lt;P&gt;2. IP layer doesn’t provide Tresos configuration. It can be configured only on Design Studio (CT).&lt;/P&gt;
&lt;P&gt;3.&amp;nbsp;&lt;U&gt;&lt;STRONG&gt;IP layer cannot be used in AUTOSAR applications, as it does not satisfy ASR compliance constraints (DEM, DET, Multicore). IP layer should not be seen as a CDD.&lt;/STRONG&gt;&lt;/U&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 22 Nov 2024 19:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/RTD-drivers-for-MC33774A/m-p/2000341#M43564</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-22T19:47:54Z</dc:date>
    </item>
  </channel>
</rss>