<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K3X8EVB-Q289 (k358 device)  Sample Driver code for QSPI module</title>
    <link>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1997428#M43417</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224386"&gt;@Ragul&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There is an example code for the Hyper Flash memory used on S32K3X8EVB-Q289 in RTD 3.0.0. Below is the path, but I will still attach it to my reply.&lt;BR clear="none" /&gt;&lt;STRONG&gt;"C:\NXP\SW32K3_RTD_4.4_R21-11_3.0.0\eclipse\plugins\Mem_43_ExFls_TS_T40D34M30I0R0\examples\S32DS\S32K358\Qspi_Ip_Example_S32K358"&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Tue, 19 Nov 2024 18:41:02 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-11-19T18:41:02Z</dc:date>
    <item>
      <title>S32K3X8EVB-Q289 (k358 device)  Sample Driver code for QSPI module</title>
      <link>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1996033#M43369</link>
      <description>&lt;P&gt;Hi, I am using&amp;nbsp;S32K3X8EVB-Q289 (k358 device) and I am not finding any example codes for this device. I need to implement QSPI for External FLash(S26KL512S) kindly do the needful ASAP. Sample driver code would be helpful.&amp;nbsp; &lt;LI-PRODUCT title="S32K3X8EVB-Q289" id="S32K3X8EVB-Q289"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Nov 2024 06:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1996033#M43369</guid>
      <dc:creator>Ragul</dc:creator>
      <dc:date>2024-11-18T06:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3X8EVB-Q289 (k358 device)  Sample Driver code for QSPI module</title>
      <link>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1997428#M43417</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224386"&gt;@Ragul&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;There is an example code for the Hyper Flash memory used on S32K3X8EVB-Q289 in RTD 3.0.0. Below is the path, but I will still attach it to my reply.&lt;BR clear="none" /&gt;&lt;STRONG&gt;"C:\NXP\SW32K3_RTD_4.4_R21-11_3.0.0\eclipse\plugins\Mem_43_ExFls_TS_T40D34M30I0R0\examples\S32DS\S32K358\Qspi_Ip_Example_S32K358"&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 18:41:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1997428#M43417</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-19T18:41:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3X8EVB-Q289 (k358 device)  Sample Driver code for QSPI module</title>
      <link>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1997695#M43425</link>
      <description>&lt;P&gt;Thanks for your support. In description of that code, it is stated that the code is applicable for&amp;nbsp;XS32K3X8&lt;STRONG&gt;CVB&lt;/STRONG&gt;-Q289 PCB 53108 RevX3 SCH RevA1 board. I need example for&amp;nbsp;S32K3X8&lt;STRONG&gt;EVB&lt;/STRONG&gt;-Q289. And can you clarify on which external flash memory it is configured on the code?? MX25L6433F or&amp;nbsp;S26KL512S ?? since&amp;nbsp;S26KL512S external flash chip is present in&amp;nbsp;S32K3X8&lt;STRONG&gt;EVB&lt;/STRONG&gt;-Q289 board.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 05:06:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1997695#M43425</guid>
      <dc:creator>Ragul</dc:creator>
      <dc:date>2024-11-20T05:06:00Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3X8EVB-Q289 (k358 device)  Sample Driver code for QSPI module</title>
      <link>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1998257#M43455</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224386"&gt;@Ragul&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The same memory is used between the two boards (&lt;SPAN&gt;S26KL512S), so you should be able to use this same example as reference without problems.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 21:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3X8EVB-Q289-k358-device-Sample-Driver-code-for-QSPI-module/m-p/1998257#M43455</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-20T21:58:55Z</dc:date>
    </item>
  </channel>
</rss>