<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K3xx - UDS over CAN Stack</title>
    <link>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997038#M43407</link>
    <description>&lt;P&gt;Is there any UDS Stack over CAN&amp;nbsp;available for S32K3xx series already ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I currently have S32K314 and I want to implement the complete the UDS Stack over CAN Bus. So I wanted to confirm if the stack is available ?&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Nov 2024 09:47:42 GMT</pubDate>
    <dc:creator>ASN7</dc:creator>
    <dc:date>2024-11-19T09:47:42Z</dc:date>
    <item>
      <title>S32K3xx - UDS over CAN Stack</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997038#M43407</link>
      <description>&lt;P&gt;Is there any UDS Stack over CAN&amp;nbsp;available for S32K3xx series already ?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I currently have S32K314 and I want to implement the complete the UDS Stack over CAN Bus. So I wanted to confirm if the stack is available ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 09:47:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997038#M43407</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2024-11-19T09:47:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - UDS over CAN Stack</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997394#M43416</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242204"&gt;@ASN7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Currently, this is the only UDS example available:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_blank"&gt;Unified bootloader Demo - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;It is an&amp;nbsp;&lt;SPAN&gt;UDS bootloader solution of S12Z, S32K1xx and S32K3xx.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 17:17:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997394#M43416</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-19T17:17:57Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - UDS over CAN Stack</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997825#M43436</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I did download the latest release from the GitHub Page and I can use the ECU-BUS, but that is just to send UDS Requests via PCAN right ? I will not be able to generate code for S32K314 right or have I understood the tool incorrectly ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 07:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1997825#M43436</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2024-11-20T07:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3xx - UDS over CAN Stack</title>
      <link>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1998248#M43454</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242204"&gt;@ASN7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;but that is just to send UDS Requests via PCAN right ?&amp;nbsp;&amp;nbsp;I will not be able to generate code for S32K314 right or have I understood the tool incorrectly ?&amp;nbsp;&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Yes, that is correct. This is simply a reference example which can be used with the S32K family.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 21:41:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3xx-UDS-over-CAN-Stack/m-p/1998248#M43454</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-20T21:41:11Z</dc:date>
    </item>
  </channel>
</rss>