<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K312 PWM generation</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-PWM-generation/m-p/1996468#M43385</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am facing the issue of PWM generation on the S32K.&lt;/P&gt;&lt;P&gt;The uC looks resetting when config frequency of PWM over 10kHz when the task is called in 10ms.&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;It is possible to generate such frequency of PWM using a 10 ms task?&lt;/LI&gt;&lt;LI&gt;Do you have any workaround to resolve the issue?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;(CORE_CLK = 120MHZ)&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Chen&lt;/P&gt;</description>
    <pubDate>Mon, 18 Nov 2024 14:17:08 GMT</pubDate>
    <dc:creator>weiweichen</dc:creator>
    <dc:date>2024-11-18T14:17:08Z</dc:date>
    <item>
      <title>S32K312 PWM generation</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PWM-generation/m-p/1996468#M43385</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am facing the issue of PWM generation on the S32K.&lt;/P&gt;&lt;P&gt;The uC looks resetting when config frequency of PWM over 10kHz when the task is called in 10ms.&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;It is possible to generate such frequency of PWM using a 10 ms task?&lt;/LI&gt;&lt;LI&gt;Do you have any workaround to resolve the issue?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;(CORE_CLK = 120MHZ)&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Chen&lt;/P&gt;</description>
      <pubDate>Mon, 18 Nov 2024 14:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PWM-generation/m-p/1996468#M43385</guid>
      <dc:creator>weiweichen</dc:creator>
      <dc:date>2024-11-18T14:17:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 PWM generation</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-PWM-generation/m-p/1997480#M43418</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/213816"&gt;@weiweichen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you provide more information about the application and connfigurations?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Tue, 19 Nov 2024 21:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-PWM-generation/m-p/1997480#M43418</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-11-19T21:58:53Z</dc:date>
    </item>
  </channel>
</rss>