<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: HARDWARE RESET or SOFTWARE RESET</title>
    <link>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1994716#M43296</link>
    <description>&lt;P&gt;&amp;nbsp;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203425"&gt;@akhilranga&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;For SW reset, please look at chapter&amp;nbsp;&lt;STRONG&gt;25.2.2.7&amp;nbsp;&lt;/STRONG&gt;from the S32K Reference Manual, it explains the reset control register.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can also use this example as reference, where a SW reset is implemented to test the ram retention:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-RAM-Retention-S32DS-R1/ta-p/1107548" target="_blank"&gt;Example S32K144 RAM Retention S32DS.R1 - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;There is also this function in the system_S32K144.c file:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1731595074372.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310591i176E29A8E88A148F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1731595074372.png" alt="Julin_AragnM_0-1731595074372.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For the watchdog, there are many community posts sharing some reference code, such as:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/WatchDog-S32k144/m-p/660503" target="_blank"&gt;Solved: WatchDog S32k144 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/watchdog-test/m-p/1469370" target="_blank"&gt;Solved: watchdog test - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;You can also refer to the examples inside the EAR SDK.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Thu, 14 Nov 2024 14:55:14 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-11-14T14:55:14Z</dc:date>
    <item>
      <title>HARDWARE RESET or SOFTWARE RESET</title>
      <link>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1993717#M43245</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;Can someone help me with enabling a Watchdog timer and also steps to initiate Software reset. I am using a S32k14x EAR SDK v0.8.6 for writing my vehicle application code. So i want to enable Watchdog timer so couldn't able to figure any knowledge base where i can get help from. And also i need help in Hardawre reset and Software Reset process.&lt;/P&gt;&lt;P&gt;It would be really helpfull if some one lends me hand here. Thanks in advance&amp;nbsp;&lt;/P&gt;&lt;P&gt;#S32K146&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 12:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1993717#M43245</guid>
      <dc:creator>akhilranga</dc:creator>
      <dc:date>2024-11-13T12:39:58Z</dc:date>
    </item>
    <item>
      <title>Re: HARDWARE RESET or SOFTWARE RESET</title>
      <link>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1994716#M43296</link>
      <description>&lt;P&gt;&amp;nbsp;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203425"&gt;@akhilranga&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;For SW reset, please look at chapter&amp;nbsp;&lt;STRONG&gt;25.2.2.7&amp;nbsp;&lt;/STRONG&gt;from the S32K Reference Manual, it explains the reset control register.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can also use this example as reference, where a SW reset is implemented to test the ram retention:&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-RAM-Retention-S32DS-R1/ta-p/1107548" target="_blank"&gt;Example S32K144 RAM Retention S32DS.R1 - NXP Community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;There is also this function in the system_S32K144.c file:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1731595074372.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/310591i176E29A8E88A148F/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1731595074372.png" alt="Julin_AragnM_0-1731595074372.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For the watchdog, there are many community posts sharing some reference code, such as:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/WatchDog-S32k144/m-p/660503" target="_blank"&gt;Solved: WatchDog S32k144 - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/S32K/watchdog-test/m-p/1469370" target="_blank"&gt;Solved: watchdog test - NXP Community&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;You can also refer to the examples inside the EAR SDK.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Thu, 14 Nov 2024 14:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1994716#M43296</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-14T14:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: HARDWARE RESET or SOFTWARE RESET</title>
      <link>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1997730#M43428</link>
      <description>&lt;P&gt;&lt;EM&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thank you for the information. &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Nov 2024 05:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HARDWARE-RESET-or-SOFTWARE-RESET/m-p/1997730#M43428</guid>
      <dc:creator>akhilranga</dc:creator>
      <dc:date>2024-11-20T05:54:40Z</dc:date>
    </item>
  </channel>
</rss>