<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Give Input from CAN to NXP Blocks in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1992737#M43170</link>
    <description>&lt;P&gt;We want to take inputs from CAN messages that is received and give these inputs to NXP blocks such as adc . pwm functions for S32k3xx.&lt;/P&gt;&lt;P&gt;Request your support as early as possible&lt;/P&gt;</description>
    <pubDate>Tue, 12 Nov 2024 09:40:24 GMT</pubDate>
    <dc:creator>Akshay_idiada</dc:creator>
    <dc:date>2024-11-12T09:40:24Z</dc:date>
    <item>
      <title>Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1992737#M43170</link>
      <description>&lt;P&gt;We want to take inputs from CAN messages that is received and give these inputs to NXP blocks such as adc . pwm functions for S32k3xx.&lt;/P&gt;&lt;P&gt;Request your support as early as possible&lt;/P&gt;</description>
      <pubDate>Tue, 12 Nov 2024 09:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1992737#M43170</guid>
      <dc:creator>Akshay_idiada</dc:creator>
      <dc:date>2024-11-12T09:40:24Z</dc:date>
    </item>
    <item>
      <title>Re: Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1993552#M43220</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;this seems to be rather application question, so it is up to user how process/use received data from CAN module.&amp;nbsp;&lt;BR /&gt;I can just recommend to refer to available RTD demo examples for CAN/ADC/PWM or refer to more examples given at&amp;nbsp;&lt;A href="https://community.nxp.com/t5/forums/recentpostspage/interaction-style/tkb/post-type/thread/board-id/S32K" target="_blank"&gt;https://community.nxp.com/t5/forums/recentpostspage/interaction-style/tkb/post-type/thread/board-id/S32K&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 09:13:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1993552#M43220</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-11-13T09:13:45Z</dc:date>
    </item>
    <item>
      <title>Re: Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1993568#M43224</link>
      <description>&lt;P&gt;Yeah that is at application side but the query is that do we have any means to provide this CAN inputs to the NXP function Blocks because these blocks read inputs from the pin directly there is no option to provide external input to these blocks.&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 09:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1993568#M43224</guid>
      <dc:creator>Akshay_idiada</dc:creator>
      <dc:date>2024-11-13T09:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1993714#M43244</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if you are asking about signal multiplexing on MCU pad then refer to chapter 4 of the device RM and device IOMUX file attached to this document, to know which peripheral function can be assigned to each MCU pad&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 13 Nov 2024 12:33:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1993714#M43244</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-11-13T12:33:56Z</dc:date>
    </item>
    <item>
      <title>Re: Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1998492#M43464</link>
      <description>Hi,&lt;BR /&gt;The examples that you are referring contains only .c files. Can you share the reference for examples that contains the Matlab models?</description>
      <pubDate>Thu, 21 Nov 2024 05:04:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/1998492#M43464</guid>
      <dc:creator>Akshay_idiada</dc:creator>
      <dc:date>2024-11-21T05:04:33Z</dc:date>
    </item>
    <item>
      <title>Re: Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/2000709#M43604</link>
      <description>Hi ,&lt;BR /&gt;Can you share the examples that contains Matlab model ?</description>
      <pubDate>Mon, 25 Nov 2024 05:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/2000709#M43604</guid>
      <dc:creator>Akshay_idiada</dc:creator>
      <dc:date>2024-11-25T05:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: Give Input from CAN to NXP Blocks</title>
      <link>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/2004204#M43740</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;check MBDT community space for more info;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt" target="_blank"&gt;https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/bd-p/mbdt&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Fri, 29 Nov 2024 08:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Give-Input-from-CAN-to-NXP-Blocks/m-p/2004204#M43740</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-11-29T08:34:41Z</dc:date>
    </item>
  </channel>
</rss>