<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックHVBMS_Integration_Project_0_8_1 not working</title>
    <link>https://community.nxp.com/t5/S32K/HVBMS-Integration-Project-0-8-1-not-working/m-p/1991411#M43083</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We're using the RD-K358BMU development board for BMS applications. We started working with the NXP reference software HVBMS_Integration_Project_0_8_1 and HVBMS_RD_Bring_up_Example_0_9_0_CD01.&lt;/P&gt;&lt;P&gt;The HVBMS_RD_Bring_up_Example_0_9_0_CD01 project worked as planned. We can observe the cell voltage in the FREEMASTER GUI.&lt;/P&gt;&lt;P&gt;However, the HVBMS_Integration_Project_0_8_1 project is not working. We were unable to see the data. The code was running, however it ended up at the error handler due to the spi timeout issue.&lt;/P&gt;&lt;P&gt;For your reference, attached the timeout handler where the SPI timeout triggered&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Balaji_KSB_0-1731289096523.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/309527i6E872D6D9FB7BC0A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Balaji_KSB_0-1731289096523.png" alt="Balaji_KSB_0-1731289096523.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Balaji.K.S&lt;/P&gt;</description>
    <pubDate>Mon, 11 Nov 2024 01:39:11 GMT</pubDate>
    <dc:creator>Balaji_KSB</dc:creator>
    <dc:date>2024-11-11T01:39:11Z</dc:date>
    <item>
      <title>HVBMS_Integration_Project_0_8_1 not working</title>
      <link>https://community.nxp.com/t5/S32K/HVBMS-Integration-Project-0-8-1-not-working/m-p/1991411#M43083</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We're using the RD-K358BMU development board for BMS applications. We started working with the NXP reference software HVBMS_Integration_Project_0_8_1 and HVBMS_RD_Bring_up_Example_0_9_0_CD01.&lt;/P&gt;&lt;P&gt;The HVBMS_RD_Bring_up_Example_0_9_0_CD01 project worked as planned. We can observe the cell voltage in the FREEMASTER GUI.&lt;/P&gt;&lt;P&gt;However, the HVBMS_Integration_Project_0_8_1 project is not working. We were unable to see the data. The code was running, however it ended up at the error handler due to the spi timeout issue.&lt;/P&gt;&lt;P&gt;For your reference, attached the timeout handler where the SPI timeout triggered&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Balaji_KSB_0-1731289096523.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/309527i6E872D6D9FB7BC0A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Balaji_KSB_0-1731289096523.png" alt="Balaji_KSB_0-1731289096523.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Balaji.K.S&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 01:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HVBMS-Integration-Project-0-8-1-not-working/m-p/1991411#M43083</guid>
      <dc:creator>Balaji_KSB</dc:creator>
      <dc:date>2024-11-11T01:39:11Z</dc:date>
    </item>
  </channel>
</rss>