<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 TJA1102 Reset</title>
    <link>https://community.nxp.com/t5/S32K/TJA1102-Reset/m-p/1991363#M43077</link>
    <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I am integrating TJA1102 with SJA1105 switch and MC S32K344.&lt;/P&gt;&lt;P&gt;Is it mandatory to issue a software reset (Bit 15) in the Basic Control Register (Register 0) after initializing the transceiver?&lt;/P&gt;&lt;P&gt;My initialization sequence is:&lt;/P&gt;&lt;P&gt;1- Set Bit 2 (CONFIG_EN) Register 17&lt;/P&gt;&lt;P&gt;2- Set Bit 0 (PHY_EN) Register 28&lt;/P&gt;&lt;P&gt;3- Set whether PHY acting as Master/Slave (Bit 15) Register 18&lt;/P&gt;&lt;P&gt;4- Clear AUTO_OP (Bit 15) in Register 28.&lt;/P&gt;&lt;P&gt;Do I need to apply Software reset (Bit 15 in Reg 0) after issuing the above initialization sequence? Also, do you recommend for any missing initializing step?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Sun, 10 Nov 2024 12:32:58 GMT</pubDate>
    <dc:creator>AhmedHamza</dc:creator>
    <dc:date>2024-11-10T12:32:58Z</dc:date>
    <item>
      <title>TJA1102 Reset</title>
      <link>https://community.nxp.com/t5/S32K/TJA1102-Reset/m-p/1991363#M43077</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I am integrating TJA1102 with SJA1105 switch and MC S32K344.&lt;/P&gt;&lt;P&gt;Is it mandatory to issue a software reset (Bit 15) in the Basic Control Register (Register 0) after initializing the transceiver?&lt;/P&gt;&lt;P&gt;My initialization sequence is:&lt;/P&gt;&lt;P&gt;1- Set Bit 2 (CONFIG_EN) Register 17&lt;/P&gt;&lt;P&gt;2- Set Bit 0 (PHY_EN) Register 28&lt;/P&gt;&lt;P&gt;3- Set whether PHY acting as Master/Slave (Bit 15) Register 18&lt;/P&gt;&lt;P&gt;4- Clear AUTO_OP (Bit 15) in Register 28.&lt;/P&gt;&lt;P&gt;Do I need to apply Software reset (Bit 15 in Reg 0) after issuing the above initialization sequence? Also, do you recommend for any missing initializing step?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Sun, 10 Nov 2024 12:32:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TJA1102-Reset/m-p/1991363#M43077</guid>
      <dc:creator>AhmedHamza</dc:creator>
      <dc:date>2024-11-10T12:32:58Z</dc:date>
    </item>
  </channel>
</rss>