<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HSE_KF_ACCESS_DEBUG_PROT attribute actual intention in S32K</title>
    <link>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1989793#M42995</link>
    <description>&lt;P&gt;It looks like you have older version of the manual. I recommend to download the latest one which is version 2.3.&lt;/P&gt;
&lt;P&gt;It's the same for non-SHE keys. If you are importing a key first time (i.e. to empty slot), it can be loaded in plain. However, if you are updating a key, it is mandatory to use encryption and/or authentication (Table 47 and 48 in RM v2.3). So, this is also trusted operation as described in the SHE, there's no difference.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Thu, 07 Nov 2024 05:52:16 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-11-07T05:52:16Z</dc:date>
    <item>
      <title>HSE_KF_ACCESS_DEBUG_PROT attribute actual intention</title>
      <link>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1984546#M42703</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In our company we are working on a project having MWCT2015S microcontroller.&lt;/P&gt;&lt;P&gt;We store keys in the HSE_B secure memory setting the&amp;nbsp;HSE_KF_ACCESS_DEBUG_PROT attribute so that the keys cannot be accessed (i.e. used) when a debugger is connected. Some of the keys may need to be updated once the product is in field (vehicle usage).&lt;/P&gt;&lt;P&gt;The question is: what does the sentence "cannot be used" include? Does it refer only to&amp;nbsp;prevent keys usage for cryptographic operations OR it means that they cannot completely handled when a debugger is connected?&lt;/P&gt;&lt;P&gt;So, is it possible to update debug protected keys when the debugger is connected?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ale_di_vi_0-1730275963982.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/307659i9CF4C31A2CD07B5C/image-size/medium?v=v2&amp;amp;px=400" alt="ale_di_vi_0-1730275963982.png" title="ale_di_vi_0-1730275963982.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance and best regards,&lt;/P&gt;&lt;P&gt;Alessandro Di Vincenzo&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 08:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1984546#M42703</guid>
      <dc:creator>ale_di_vi</dc:creator>
      <dc:date>2024-10-30T08:15:11Z</dc:date>
    </item>
    <item>
      <title>Re: HSE_KF_ACCESS_DEBUG_PROT attribute actual intention</title>
      <link>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1986287#M42813</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218511"&gt;@ale_di_vi&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;here is an explanation from SHE specification:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1730467558420.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308178iC38BE088C86EA433/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1730467558420.png" alt="lukaszadrapa_0-1730467558420.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1730467558420.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 13:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1986287#M42813</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-11-01T13:26:24Z</dc:date>
    </item>
    <item>
      <title>Re: HSE_KF_ACCESS_DEBUG_PROT attribute actual intention</title>
      <link>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1986965#M42863</link>
      <description>Hi Lukas,&lt;BR /&gt;We don't store the key in its SHE-format. Can I consider this statement valid also for the non-SHE keys managed according to table 31 in chapter 7.1.4.2 from the HSE_B RM?&lt;BR /&gt;Thank you in advance,&lt;BR /&gt;Alessandro</description>
      <pubDate>Mon, 04 Nov 2024 10:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1986965#M42863</guid>
      <dc:creator>ale_di_vi</dc:creator>
      <dc:date>2024-11-04T10:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: HSE_KF_ACCESS_DEBUG_PROT attribute actual intention</title>
      <link>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1989793#M42995</link>
      <description>&lt;P&gt;It looks like you have older version of the manual. I recommend to download the latest one which is version 2.3.&lt;/P&gt;
&lt;P&gt;It's the same for non-SHE keys. If you are importing a key first time (i.e. to empty slot), it can be loaded in plain. However, if you are updating a key, it is mandatory to use encryption and/or authentication (Table 47 and 48 in RM v2.3). So, this is also trusted operation as described in the SHE, there's no difference.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 05:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1989793#M42995</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-11-07T05:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: HSE_KF_ACCESS_DEBUG_PROT attribute actual intention</title>
      <link>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1989972#M43009</link>
      <description>Ok, got it: debug protection flag is not a problem for key update.&lt;BR /&gt;Thank you Lukas</description>
      <pubDate>Thu, 07 Nov 2024 08:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/HSE-KF-ACCESS-DEBUG-PROT-attribute-actual-intention/m-p/1989972#M43009</guid>
      <dc:creator>ale_di_vi</dc:creator>
      <dc:date>2024-11-07T08:17:49Z</dc:date>
    </item>
  </channel>
</rss>