<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I2C Four-Wire Scheme in S32K</title>
    <link>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1989027#M42974</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242204"&gt;@ASN7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, that is correct.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 16:08:17 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2024-11-06T16:08:17Z</dc:date>
    <item>
      <title>I2C Four-Wire Scheme</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1983603#M42641</link>
      <description>&lt;P&gt;I'm working with a S32K314 on a custom board and have connected a temperature sensor to the SDAS and SCLS lines for I2C communication. This sensor is the only I2C device, and it isn’t connected to any other I2C lines. I wish to use LPSPI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;From my understanding of the manual (image below), it appears that SDAS and SCLS are secondary lines. Could someone confirm if these lines are suitable for a Two-Wire I2C scheme with my temperature sensor, or if I should be using the primary SDA and SCL lines instead?&lt;/P&gt;&lt;P&gt;Thanks in advance for any clarification!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ASN7_0-1730189638617.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/307420iECDF58C4DD6C52D6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ASN7_0-1730189638617.png" alt="ASN7_0-1730189638617.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;ASN7_0-1730189638617.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 08:17:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1983603#M42641</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2024-10-29T08:17:07Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Four-Wire Scheme</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1984088#M42668</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242204"&gt;@ASN7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The four-wire scheme, instead of using traditional I2C SDA\SCL bidirectional lines, it adds an option to split them into input and output functionality. This in order to improve the noise immunity of the I2C bus.&lt;/P&gt;
&lt;P&gt;This change can be implemented with two transistors, six resistors, and two diodes. You can see a recommended connection diagram in the same chapter:&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1730227650471.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/307523iC51007376241AE4E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1730227650471.png" alt="Julin_AragnM_0-1730227650471.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Julin_AragnM_0-1730227650471.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;This implementation choice is dependent on your application. You must weigh the benefit of the robustness against the&amp;nbsp;additional system BOM costs.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If this is not critical or safety implementation, the traditional two-wire configuration should be enough for most sensors.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 18:49:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1984088#M42668</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-10-29T18:49:29Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Four-Wire Scheme</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1988860#M42970</link>
      <description>&lt;P&gt;So to conclude your answer, it would not be possible to only use SDAS and SCLS pins. I would have to connect SDA and SCL as well in order to use SDAS and SCLS.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I hope my understanding is correct. Thank you.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 12:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1988860#M42970</guid>
      <dc:creator>ASN7</dc:creator>
      <dc:date>2024-11-06T12:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: I2C Four-Wire Scheme</title>
      <link>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1989027#M42974</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242204"&gt;@ASN7&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, that is correct.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 16:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/I2C-Four-Wire-Scheme/m-p/1989027#M42974</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-11-06T16:08:17Z</dc:date>
    </item>
  </channel>
</rss>