<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: EEPROM LOST OR FAIL</title>
    <link>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1988596#M42959</link>
    <description>&lt;P&gt;Could you specify used product?&lt;/P&gt;</description>
    <pubDate>Wed, 06 Nov 2024 07:56:03 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2024-11-06T07:56:03Z</dc:date>
    <item>
      <title>EEPROM LOST OR FAIL</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1987727#M42899</link>
      <description>&lt;P&gt;hello,experts:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; We are updating the APP via UDS protocol and recording the number of updates in the EEPROM, we have executed it more than 3000 times in total with one failure in between. The last read count is only about 800 times, we suspect that the EEprom has failed to write due to some factor resulting in data loss, what are the factors that may cause the EEPROM to lose or fail?&lt;/P&gt;</description>
      <pubDate>Tue, 05 Nov 2024 07:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1987727#M42899</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-11-05T07:09:17Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM LOST OR FAIL</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1987744#M42904</link>
      <description>when failed ,we found the eeprom data is 0</description>
      <pubDate>Tue, 05 Nov 2024 07:29:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1987744#M42904</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-11-05T07:29:37Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM LOST OR FAIL</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1988596#M42959</link>
      <description>&lt;P&gt;Could you specify used product?&lt;/P&gt;</description>
      <pubDate>Wed, 06 Nov 2024 07:56:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1988596#M42959</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-11-06T07:56:03Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM LOST OR FAIL</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1989569#M42980</link>
      <description>&lt;P&gt;S32K116&lt;/P&gt;</description>
      <pubDate>Thu, 07 Nov 2024 00:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1989569#M42980</guid>
      <dc:creator>PINKMAN</dc:creator>
      <dc:date>2024-11-07T00:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM LOST OR FAIL</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1991175#M43070</link>
      <description>&lt;P&gt;In general ECC error in FLASH may have following reason:&lt;BR /&gt;- Unexpected reset during flash erase or flash program operation&lt;BR /&gt;- Wear out of particular flash sector = number of program/erase cycles that device’s flash is capable to withstand is exceeded (in practice, real endurance is greater than specified minimum).&lt;BR /&gt;- Over-programming of particular flash area that is programming without erasing. It is basically software fault.&lt;BR /&gt;- Soft error (radiation, electro-magnetic interference, or electrical noise) during reading or executing from flash memory&lt;/P&gt;
&lt;P&gt;As EEEPROM state machine is autonomous, over-programming does not happen.&lt;BR /&gt;Unexpected reset is typical reason of loosing data, EEEPROM is capable to restore previous data.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 15:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-LOST-OR-FAIL/m-p/1991175#M43070</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-11-08T15:55:03Z</dc:date>
    </item>
  </channel>
</rss>