<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Checking Core Configuration Mode on S32K344 Q172 EVB (Lockstep/Dual-Core) in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Checking-Core-Configuration-Mode-on-S32K344-Q172-EVB-Lockstep/m-p/1987311#M42882</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242059"&gt;@Shivaprasad_sp&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To check the chip's operating mode (Lockstep or Decoupled) you can read bit 29 (LOCKSTEP_EN) of the DCM_GPR -&amp;gt; DCMROF19 register. This bit returns the operation mode as configured in the DCF record (UTEST_MISC[LOCKSTEP_EN]).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
    <pubDate>Mon, 04 Nov 2024 20:42:04 GMT</pubDate>
    <dc:creator>VaneB</dc:creator>
    <dc:date>2024-11-04T20:42:04Z</dc:date>
    <item>
      <title>Checking Core Configuration Mode on S32K344 Q172 EVB (Lockstep/Dual-Core)</title>
      <link>https://community.nxp.com/t5/S32K/Checking-Core-Configuration-Mode-on-S32K344-Q172-EVB-Lockstep/m-p/1987027#M42864</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm currently working on a project using the S32K344 Q172 EVB and I need to determine whether the MCU is configured in lockstep mode or dual-core mode. Is there a way to read or verify the core configuration mode that the S32K344 is set to? Any pointers on the registers or methods to check this information&lt;/P&gt;</description>
      <pubDate>Mon, 04 Nov 2024 12:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Checking-Core-Configuration-Mode-on-S32K344-Q172-EVB-Lockstep/m-p/1987027#M42864</guid>
      <dc:creator>Shivaprasad_sp</dc:creator>
      <dc:date>2024-11-04T12:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: Checking Core Configuration Mode on S32K344 Q172 EVB (Lockstep/Dual-Core)</title>
      <link>https://community.nxp.com/t5/S32K/Checking-Core-Configuration-Mode-on-S32K344-Q172-EVB-Lockstep/m-p/1987311#M42882</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242059"&gt;@Shivaprasad_sp&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To check the chip's operating mode (Lockstep or Decoupled) you can read bit 29 (LOCKSTEP_EN) of the DCM_GPR -&amp;gt; DCMROF19 register. This bit returns the operation mode as configured in the DCF record (UTEST_MISC[LOCKSTEP_EN]).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, VaneB&lt;/P&gt;</description>
      <pubDate>Mon, 04 Nov 2024 20:42:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Checking-Core-Configuration-Mode-on-S32K344-Q172-EVB-Lockstep/m-p/1987311#M42882</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-11-04T20:42:04Z</dc:date>
    </item>
  </channel>
</rss>