<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K3 Flexcan FIFO MB in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K3-Flexcan-FIFO-MB/m-p/1986898#M42858</link>
    <description>&lt;P&gt;&lt;A href="mailto:Hi@Jon123" target="_blank"&gt;Hi@Jon123&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This area is reserved for internal use of the Legacy RX FIFO engine,&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1730709949873.png" style="width: 636px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308362i09225F6A768EB6B4/image-dimensions/636x652?v=v2" width="636" height="652" role="button" title="Senlent_0-1730709949873.png" alt="Senlent_0-1730709949873.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 04 Nov 2024 08:51:56 GMT</pubDate>
    <dc:creator>Senlent</dc:creator>
    <dc:date>2024-11-04T08:51:56Z</dc:date>
    <item>
      <title>S32K3 Flexcan FIFO MB</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Flexcan-FIFO-MB/m-p/1986143#M42803</link>
      <description>&lt;P&gt;Page 38 of&amp;nbsp;RTD_CAN_43_FLEXCAN_UM.pdf：&lt;/P&gt;&lt;P&gt;*****************************************&lt;/P&gt;&lt;P&gt;3.6.3 Legacy Rx FIFO Configuration The receive-only FIFO is enabled for specific controller by&lt;BR /&gt;asserting the FEN bit in the MCR register. The Legacy RxFifo configuration in the Tresos plugin is implemented&lt;BR /&gt;by selection CanRxFiFo tab to CanLegacyFiFo in CanRxFiFo container.&lt;BR /&gt;When the Fifo is enabled, the memory region normally occupied by the first 6 MBs is normally reserved for use of&lt;BR /&gt;the Fifo engine. The CPU can read the received frames sequentially, in the order they were received, by repeatedly&lt;BR /&gt;accessing the MB0 structure.&lt;BR /&gt;The interrupts corresponding to MB0 to 5 have a different behavior when Rx Fifo in enabled. Bit 7 of the IFLAG1&lt;BR /&gt;becomes the “Fifo Overflow” flag, bit 6 becomes the “Fifo Warning” flag, bit 5 becomes the “Frame Available in Rx&lt;BR /&gt;Fifo” flag and bits 4 to 0 are unused. If Legacy RxFifo is enabled for a specific controller, the user shall configure at&lt;BR /&gt;least 1 hardware object which use that controller.&lt;/P&gt;&lt;P&gt;*****************************************&lt;/P&gt;&lt;P&gt;As far as I know, when Legacy RX FIFO is activated, the RAM where the first six standard X mailboxes are located becomes six RX FIFO in depth, and then becomes a Filter table element. Combined with the diagram in the above RTD_CAN_43_FLEXCAN_UM manual and the practical application, it can be seen that only MB0 is being used, so the other five MB's functions are different in the UM manual, but I can't find the specific functions of the other five MB's, that is, M1-M5. Can you answer my doubts? Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 08:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Flexcan-FIFO-MB/m-p/1986143#M42803</guid>
      <dc:creator>Jon123</dc:creator>
      <dc:date>2024-11-01T08:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K3 Flexcan FIFO MB</title>
      <link>https://community.nxp.com/t5/S32K/S32K3-Flexcan-FIFO-MB/m-p/1986898#M42858</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Jon123" target="_blank"&gt;Hi@Jon123&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This area is reserved for internal use of the Legacy RX FIFO engine,&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1730709949873.png" style="width: 636px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/308362i09225F6A768EB6B4/image-dimensions/636x652?v=v2" width="636" height="652" role="button" title="Senlent_0-1730709949873.png" alt="Senlent_0-1730709949873.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Nov 2024 08:51:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K3-Flexcan-FIFO-MB/m-p/1986898#M42858</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-11-04T08:51:56Z</dc:date>
    </item>
  </channel>
</rss>