<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN s32k358 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-s32k358/m-p/1985775#M42785</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I know there is no S32K358 CAN example available, except for a loopback example. When I enable the pins, I encounter many errors.&lt;/P&gt;&lt;P&gt;So, I decided to create my own example from scratch. I have attached the project here. Could someone help me get it working? I successfully created a similar example for the S32K344, which works fine. However, the same approach doesn’t work for the S32K358. I am using the HVBMS 800V evaluation board, while the S32K344 was used with the HVBMS 400V.&lt;/P&gt;&lt;P&gt;It’s very strange because it’s the same example. I used the same configuration, although the pins are different, but nothing appears in our Peak CAN viewer. I set a breakpoint in my&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;CanIf_RxIndication&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;function and I see some real data being received, but nothing in the TX. I did some debugging, but nothing is clear.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Thu, 31 Oct 2024 20:18:56 GMT</pubDate>
    <dc:creator>AchrafOukheir</dc:creator>
    <dc:date>2024-10-31T20:18:56Z</dc:date>
    <item>
      <title>CAN s32k358</title>
      <link>https://community.nxp.com/t5/S32K/CAN-s32k358/m-p/1985775#M42785</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I know there is no S32K358 CAN example available, except for a loopback example. When I enable the pins, I encounter many errors.&lt;/P&gt;&lt;P&gt;So, I decided to create my own example from scratch. I have attached the project here. Could someone help me get it working? I successfully created a similar example for the S32K344, which works fine. However, the same approach doesn’t work for the S32K358. I am using the HVBMS 800V evaluation board, while the S32K344 was used with the HVBMS 400V.&lt;/P&gt;&lt;P&gt;It’s very strange because it’s the same example. I used the same configuration, although the pins are different, but nothing appears in our Peak CAN viewer. I set a breakpoint in my&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;CanIf_RxIndication&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;function and I see some real data being received, but nothing in the TX. I did some debugging, but nothing is clear.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 20:18:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-s32k358/m-p/1985775#M42785</guid>
      <dc:creator>AchrafOukheir</dc:creator>
      <dc:date>2024-10-31T20:18:56Z</dc:date>
    </item>
    <item>
      <title>Re: CAN s32k358</title>
      <link>https://community.nxp.com/t5/S32K/CAN-s32k358/m-p/1986155#M42804</link>
      <description>&lt;DIV&gt;Hi,&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;if module is able to receive a message but not successfully send, it can point to CAN bit timing issue.&lt;/DIV&gt;
&lt;DIV&gt;Try to check module MCR/ECR/ESR1 registers for any error detected. Also it could be fine you measure transceiver TX/RX and CAN lines to know a real behavior.&lt;/DIV&gt;
&lt;DIV&gt;What I can recommend more is to not using FIRC and CAN PE clock. Select different one not using FIRC and recalculate CAN bit timing.&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;BR, Petr&lt;/DIV&gt;</description>
      <pubDate>Fri, 01 Nov 2024 09:01:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-s32k358/m-p/1986155#M42804</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-11-01T09:01:19Z</dc:date>
    </item>
  </channel>
</rss>