<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Questions about the random number generator function in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1985741#M42783</link>
    <description>That's right, I was asking about the CSEc on the S32K. Thanks for the help! My question is all cleared up</description>
    <pubDate>Thu, 31 Oct 2024 18:17:39 GMT</pubDate>
    <dc:creator>Derek_Yoon</dc:creator>
    <dc:date>2024-10-31T18:17:39Z</dc:date>
    <item>
      <title>Questions about the random number generator function</title>
      <link>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1984173#M42672</link>
      <description>&lt;P&gt;Hello teams.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Hope all is well&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I saw an NXP engineer's response to a TRNG related question on this board that "TRNG operates internally to generate the seed from which the PRNG is built."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So, does that mean there is no need to input a separate seed value to generate a random number?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Ps :&amp;nbsp; I know that when using the DRBG algorithm, it need to input a seed with a certain entropy.&amp;nbsp;Are the DRBG algorithm and PRNG different concepts?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Oct 2024 20:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1984173#M42672</guid>
      <dc:creator>Derek_Yoon</dc:creator>
      <dc:date>2024-10-29T20:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about the random number generator function</title>
      <link>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1985727#M42782</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242691"&gt;@Derek_Yoon&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are we talking about CSEc on S32K1? It's given by SHE specification. Initial seed is generated by CMD_INIT_RNG command. Then you can generate random numbers while it is not necessary to reseed. The only additional thing you can do in runtime is to run CMD_EXTEND_SEED command to supply 128 bit of entropy. You can call this command whenever additional entropy is needed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 17:30:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1985727#M42782</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-10-31T17:30:59Z</dc:date>
    </item>
    <item>
      <title>Re: Questions about the random number generator function</title>
      <link>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1985741#M42783</link>
      <description>That's right, I was asking about the CSEc on the S32K. Thanks for the help! My question is all cleared up</description>
      <pubDate>Thu, 31 Oct 2024 18:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Questions-about-the-random-number-generator-function/m-p/1985741#M42783</guid>
      <dc:creator>Derek_Yoon</dc:creator>
      <dc:date>2024-10-31T18:17:39Z</dc:date>
    </item>
  </channel>
</rss>