<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: update S32DS plugin GNU ARM PEmicro interface OFFLINE.</title>
    <link>https://community.nxp.com/t5/S32K/update-S32DS-plugin-GNU-ARM-PEmicro-interface-OFFLINE/m-p/1981860#M42530</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I don't know which version of RTD you have installed, so I'm not sure which version of S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices I would recommend you install.&lt;/P&gt;
&lt;P&gt;If you installed S32K3 RTD 3.0.0, please refer to&amp;nbsp;the step3 of&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K3-RTD-3-0-0-in-S32DS-v3-5/ta-p/1753870" target="_self"&gt;&amp;nbsp;HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5&lt;/A&gt;.&lt;BR /&gt;If you installed S32K3 RTD 4.0.0, please refer to&amp;nbsp;the step3 of&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/RTD-4-0-with-Design-Studio-3-5/m-p/1846501#M34160" target="_self"&gt;RTD 4.0 with Design Studio 3.5&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
    <pubDate>Fri, 25 Oct 2024 08:20:27 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-10-25T08:20:27Z</dc:date>
    <item>
      <title>update S32DS plugin GNU ARM PEmicro interface OFFLINE.</title>
      <link>https://community.nxp.com/t5/S32K/update-S32DS-plugin-GNU-ARM-PEmicro-interface-OFFLINE/m-p/1979736#M42408</link>
      <description>&lt;P&gt;Hi~&lt;/P&gt;&lt;P&gt;When using S32DS, I found that the chip list of PEdebugger in the project configuration did not have the chip model I expected (s32k324_SECUREDEBUG). I want to upgrade the relevant plug-in version (GNU ARM PEmicro interface Debugging Support). Because I am in a limited network environment, I can only update offline. Where can I download the offline upgrade package of this plug-in?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;thank you~&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 03:52:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/update-S32DS-plugin-GNU-ARM-PEmicro-interface-OFFLINE/m-p/1979736#M42408</guid>
      <dc:creator>zxdd</dc:creator>
      <dc:date>2024-10-23T03:52:37Z</dc:date>
    </item>
    <item>
      <title>Re: update S32DS plugin GNU ARM PEmicro interface OFFLINE.</title>
      <link>https://community.nxp.com/t5/S32K/update-S32DS-plugin-GNU-ARM-PEmicro-interface-OFFLINE/m-p/1981860#M42530</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I don't know which version of RTD you have installed, so I'm not sure which version of S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices I would recommend you install.&lt;/P&gt;
&lt;P&gt;If you installed S32K3 RTD 3.0.0, please refer to&amp;nbsp;the step3 of&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K3-RTD-3-0-0-in-S32DS-v3-5/ta-p/1753870" target="_self"&gt;&amp;nbsp;HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5&lt;/A&gt;.&lt;BR /&gt;If you installed S32K3 RTD 4.0.0, please refer to&amp;nbsp;the step3 of&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/RTD-4-0-with-Design-Studio-3-5/m-p/1846501#M34160" target="_self"&gt;RTD 4.0 with Design Studio 3.5&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Fri, 25 Oct 2024 08:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/update-S32DS-plugin-GNU-ARM-PEmicro-interface-OFFLINE/m-p/1981860#M42530</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-10-25T08:20:27Z</dc:date>
    </item>
  </channel>
</rss>