<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 and DFlash/PFlash prefetch buffer in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-and-DFlash-PFlash-prefetch-buffer/m-p/888366#M4236</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Enrico,&lt;/P&gt;&lt;P&gt;The Flash commands do not update the content of the buffers.&lt;BR /&gt;For example, with the buffers enabled, if a PFlash address is read, then reprogrammed and read again, both read accesses will return the same data. &lt;BR /&gt;Because the single-entry buffer can store the previously read data (Section 35.2.1 RM, rev.9).&lt;BR /&gt;So, this is on the user’s responsibility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Mar 2019 19:36:51 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2019-03-12T19:36:51Z</dc:date>
    <item>
      <title>S32K144 and DFlash/PFlash prefetch buffer</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-and-DFlash-PFlash-prefetch-buffer/m-p/888365#M4235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;when I write DFlash/PFash memory (with FCCOB registers) is it mandatory to disable the respective prefetch buffers?&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;E.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 17:47:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-and-DFlash-PFlash-prefetch-buffer/m-p/888365#M4235</guid>
      <dc:creator>enricoantonioli</dc:creator>
      <dc:date>2019-03-12T17:47:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 and DFlash/PFlash prefetch buffer</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-and-DFlash-PFlash-prefetch-buffer/m-p/888366#M4236</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Enrico,&lt;/P&gt;&lt;P&gt;The Flash commands do not update the content of the buffers.&lt;BR /&gt;For example, with the buffers enabled, if a PFlash address is read, then reprogrammed and read again, both read accesses will return the same data. &lt;BR /&gt;Because the single-entry buffer can store the previously read data (Section 35.2.1 RM, rev.9).&lt;BR /&gt;So, this is on the user’s responsibility.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 19:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-and-DFlash-PFlash-prefetch-buffer/m-p/888366#M4236</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2019-03-12T19:36:51Z</dc:date>
    </item>
  </channel>
</rss>