<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Flexcan test issues on FPGA board in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Flexcan-test-issues-on-FPGA-board/m-p/1978197#M42320</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;which devices are used in fact? You have some FPGA connected to S32K device, or what?&lt;BR /&gt;It would be great you share screenshots for&amp;nbsp;&lt;SPAN&gt;unexpected can frames and errors detected.&lt;/SPAN&gt;&lt;BR /&gt;A behavior can indicate inconsistent CAN bit timing used on CAN bus. Be sure all nodes connected use a same bit timing.&lt;BR /&gt;For 40MHz PE clock and 4Mbps set TDC offset higher, i.e. 6-8.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Mon, 21 Oct 2024 11:33:15 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-10-21T11:33:15Z</dc:date>
    <item>
      <title>Flexcan test issues on FPGA board</title>
      <link>https://community.nxp.com/t5/S32K/Flexcan-test-issues-on-FPGA-board/m-p/1976508#M42247</link>
      <description>&lt;P&gt;Hi dears:&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have met some flexcan issues on my FPAG board&lt;/P&gt;&lt;P&gt;test enviroment : FPGA core frequency is 32M， flexcan peripheral clock and oscillator clock are both collect to 40M， the software is contiously send canfd frames:&lt;/P&gt;&lt;P&gt;1. when I configure a baudrate with 500K + 2M， there is no problem&lt;/P&gt;&lt;P&gt;2. when I configure a baudrate with 1M + 2M， there are some "unexpected can frames" occured on the bus (I use logic analyzer to watch them),&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2.1 the canfd frames is send out as expected&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2.2 the can frame is&amp;nbsp;immediately(11 bits) followed by the canfd frame&lt;/P&gt;&lt;P&gt;&amp;nbsp; 2.3 flexcan will report bit error when send these can frames&lt;/P&gt;&lt;P&gt;3. when I configure a baudrate with 500K + 4M/5M, the TDC is on, and TDC offset is 3&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;there is only one frame send out, and there is no error report , I have watch the MB SRAM, the MB cs code is always "TX DATA," no update .&lt;/P&gt;&lt;P&gt;wish to hear from you, thanks !&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 02:22:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flexcan-test-issues-on-FPGA-board/m-p/1976508#M42247</guid>
      <dc:creator>karsen</dc:creator>
      <dc:date>2024-10-18T02:22:58Z</dc:date>
    </item>
    <item>
      <title>Re: Flexcan test issues on FPGA board</title>
      <link>https://community.nxp.com/t5/S32K/Flexcan-test-issues-on-FPGA-board/m-p/1978197#M42320</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;which devices are used in fact? You have some FPGA connected to S32K device, or what?&lt;BR /&gt;It would be great you share screenshots for&amp;nbsp;&lt;SPAN&gt;unexpected can frames and errors detected.&lt;/SPAN&gt;&lt;BR /&gt;A behavior can indicate inconsistent CAN bit timing used on CAN bus. Be sure all nodes connected use a same bit timing.&lt;BR /&gt;For 40MHz PE clock and 4Mbps set TDC offset higher, i.e. 6-8.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 11:33:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flexcan-test-issues-on-FPGA-board/m-p/1978197#M42320</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-10-21T11:33:15Z</dc:date>
    </item>
  </channel>
</rss>