<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Delay between frames on LPSPI</title>
    <link>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976790#M42263</link>
    <description>&lt;P&gt;Yes, this was it, I was using default timings in Tresos SPI configuration because i thought they are not taken into consideration since I'm not using CS driven by SPI engine but the GPIO.&lt;/P&gt;&lt;P&gt;Thanks a lot, have a nice day&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Oct 2024 07:28:24 GMT</pubDate>
    <dc:creator>Grzechu81</dc:creator>
    <dc:date>2024-10-18T07:28:24Z</dc:date>
    <item>
      <title>Delay between frames on LPSPI</title>
      <link>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976038#M42212</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;uC: MWCT2016S (S32K312)&lt;/P&gt;&lt;P&gt;When using 32 bit data width for ExternalBuffer in SPI Channel configuration I've noticed that there is still a 6us delay between 4 bytes frames on SPI (see attachment).&lt;/P&gt;&lt;P&gt;Interesting thing is that delay length is the same as frame length (6,23 us).&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;Spi_SyncTransmit API.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;How to get rid (if possible) of this delay ?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 11:31:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976038#M42212</guid>
      <dc:creator>Grzechu81</dc:creator>
      <dc:date>2024-10-17T11:31:24Z</dc:date>
    </item>
    <item>
      <title>Re: Delay between frames on LPSPI</title>
      <link>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976191#M42231</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/211267"&gt;@Grzechu81&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;you need to setup LPSPI CCR1 register - field PCSPCS - please find detailed description in S32K3 RM rev9, chapter 70.6.1.13 .&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 15:08:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976191#M42231</guid>
      <dc:creator>PavelL</dc:creator>
      <dc:date>2024-10-17T15:08:53Z</dc:date>
    </item>
    <item>
      <title>Re: Delay between frames on LPSPI</title>
      <link>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976790#M42263</link>
      <description>&lt;P&gt;Yes, this was it, I was using default timings in Tresos SPI configuration because i thought they are not taken into consideration since I'm not using CS driven by SPI engine but the GPIO.&lt;/P&gt;&lt;P&gt;Thanks a lot, have a nice day&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 07:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Delay-between-frames-on-LPSPI/m-p/1976790#M42263</guid>
      <dc:creator>Grzechu81</dc:creator>
      <dc:date>2024-10-18T07:28:24Z</dc:date>
    </item>
  </channel>
</rss>