<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K322 dual-core compilation problem</title>
    <link>https://community.nxp.com/t5/S32K/S32K322-dual-core-compilation-problem/m-p/1976780#M42261</link>
    <description>&lt;P&gt;Dears；&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;We adopt the NXP S32K322 solution and use PE U-MULTILINK as the tool. On this product, we need to run FreeRTOS separately on M7-0 and M7_1. Currently, we have compiled the program separately for M7-0 or M7_1, and both have been approved; But after adding the official FreeRTOS to the project, it is necessary to compile M7-0 and M7_1. Currently, only the M7-0 core project can be compiled, and the M7_1 core project cannot be compiled. What modifications or configurations are required to compile the M7_1 FreeRTOS software simultaneously? thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;The printing information is as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;real-ld.exe: S32K322_Multicode_TEST_M7_1.elf section `.sram_bss' will not fit in region&amp;nbsp; &amp;nbsp;`int_sram_c1'&lt;/P&gt;&lt;P&gt;real-ld.exe: section .non_cacheable_data VMA [20408000,20408103] overlaps section .sram_bss VMA [2040610c,204083bf]&lt;/P&gt;&lt;P&gt;real-ld.exe: section .heap VMA [204083c0,204093bf] overlaps section .non_cacheable_bss VMA [20408104,2040856b]&lt;/P&gt;&lt;P&gt;real-ld.exe: region `int_sram_c1' overflowed by 5312 bytes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Best Regards！&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 18 Oct 2024 07:19:35 GMT</pubDate>
    <dc:creator>jack_huang1</dc:creator>
    <dc:date>2024-10-18T07:19:35Z</dc:date>
    <item>
      <title>S32K322 dual-core compilation problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K322-dual-core-compilation-problem/m-p/1976780#M42261</link>
      <description>&lt;P&gt;Dears；&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;We adopt the NXP S32K322 solution and use PE U-MULTILINK as the tool. On this product, we need to run FreeRTOS separately on M7-0 and M7_1. Currently, we have compiled the program separately for M7-0 or M7_1, and both have been approved; But after adding the official FreeRTOS to the project, it is necessary to compile M7-0 and M7_1. Currently, only the M7-0 core project can be compiled, and the M7_1 core project cannot be compiled. What modifications or configurations are required to compile the M7_1 FreeRTOS software simultaneously? thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;The printing information is as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;real-ld.exe: S32K322_Multicode_TEST_M7_1.elf section `.sram_bss' will not fit in region&amp;nbsp; &amp;nbsp;`int_sram_c1'&lt;/P&gt;&lt;P&gt;real-ld.exe: section .non_cacheable_data VMA [20408000,20408103] overlaps section .sram_bss VMA [2040610c,204083bf]&lt;/P&gt;&lt;P&gt;real-ld.exe: section .heap VMA [204083c0,204093bf] overlaps section .non_cacheable_bss VMA [20408104,2040856b]&lt;/P&gt;&lt;P&gt;real-ld.exe: region `int_sram_c1' overflowed by 5312 bytes&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Best Regards！&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 07:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K322-dual-core-compilation-problem/m-p/1976780#M42261</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2024-10-18T07:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: S32K322 dual-core compilation problem</title>
      <link>https://community.nxp.com/t5/S32K/S32K322-dual-core-compilation-problem/m-p/1980896#M42465</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/137206"&gt;@jack_huang1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;According to the error message, you are running out of RAM. It's necessary to update the linker file. The message says that int_sram_c1 is too small. So, you need to enlarge this section - at the cost of other section(s).&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 06:45:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K322-dual-core-compilation-problem/m-p/1980896#M42465</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-10-24T06:45:17Z</dc:date>
    </item>
  </channel>
</rss>