<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Get specified temperature range for S32K116 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Get-specified-temperature-range-for-S32K116/m-p/887984#M4219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a S32K116 MCU with extended temperature range (-40...125°C) for my current project. I would like to detect if a wrong chip with the lower temperature range is assembled, because this could lead to expensive loss of function in the field.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a register inside the chip that contains the temperature range information like the registers that contain information about the chip features (SIM-&amp;gt;SDID)?&lt;/P&gt;&lt;P&gt;If not, is there some other way to detect the specified temperature range in software?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Mar 2019 12:37:35 GMT</pubDate>
    <dc:creator>markus1</dc:creator>
    <dc:date>2019-03-12T12:37:35Z</dc:date>
    <item>
      <title>Get specified temperature range for S32K116</title>
      <link>https://community.nxp.com/t5/S32K/Get-specified-temperature-range-for-S32K116/m-p/887984#M4219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a S32K116 MCU with extended temperature range (-40...125°C) for my current project. I would like to detect if a wrong chip with the lower temperature range is assembled, because this could lead to expensive loss of function in the field.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a register inside the chip that contains the temperature range information like the registers that contain information about the chip features (SIM-&amp;gt;SDID)?&lt;/P&gt;&lt;P&gt;If not, is there some other way to detect the specified temperature range in software?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Markus&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 12:37:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Get-specified-temperature-range-for-S32K116/m-p/887984#M4219</guid>
      <dc:creator>markus1</dc:creator>
      <dc:date>2019-03-12T12:37:35Z</dc:date>
    </item>
    <item>
      <title>Re: Get specified temperature range for S32K116</title>
      <link>https://community.nxp.com/t5/S32K/Get-specified-temperature-range-for-S32K116/m-p/887985#M4220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I don't think it would be possible to detect it SW way. Such information is not stored in any MCU's register.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 18:28:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Get-specified-temperature-range-for-S32K116/m-p/887985#M4220</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-03-12T18:28:19Z</dc:date>
    </item>
  </channel>
</rss>