<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: OTA_S32K144_Use_Case_WS Access</title>
    <link>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1975311#M42170</link>
    <description>Thank you! I really appreciate it.</description>
    <pubDate>Wed, 16 Oct 2024 15:16:10 GMT</pubDate>
    <dc:creator>aipers</dc:creator>
    <dc:date>2024-10-16T15:16:10Z</dc:date>
    <item>
      <title>OTA_S32K144_Use_Case_WS Access</title>
      <link>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1972800#M41993</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was reading AN 12323 "S32kxx Firmware Updates" and was interested in trying out the demo where they do a firmware update using a bootloader and CAN across two partitioned devices. Anyone know where I can get access to the demo workspace:&amp;nbsp;OTA_S32K144_Use_Case_WS?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, I notice in the project they are debugging with DEBUG_RAM, I have always done DEBUG_FLASH, is there an important difference that will cause errors if I do one or the other?&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Sun, 13 Oct 2024 15:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1972800#M41993</guid>
      <dc:creator>aipers</dc:creator>
      <dc:date>2024-10-13T15:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: OTA_S32K144_Use_Case_WS Access</title>
      <link>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1975244#M42166</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241896"&gt;@aipers&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the software can be downloaded here:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip" target="_blank"&gt;https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Only the S32K144_Memory_Partition project should be executed from RAM memory. Here is the reason:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1729087922089.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/305035iCE139B83A772B0F9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1729087922089.png" alt="lukaszadrapa_0-1729087922089.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1729087922089.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Other projects should be programmed to the flash.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 14:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1975244#M42166</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-10-16T14:13:03Z</dc:date>
    </item>
    <item>
      <title>Re: OTA_S32K144_Use_Case_WS Access</title>
      <link>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1975311#M42170</link>
      <description>Thank you! I really appreciate it.</description>
      <pubDate>Wed, 16 Oct 2024 15:16:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/OTA-S32K144-Use-Case-WS-Access/m-p/1975311#M42170</guid>
      <dc:creator>aipers</dc:creator>
      <dc:date>2024-10-16T15:16:10Z</dc:date>
    </item>
  </channel>
</rss>