<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Initialize NfcLib_Init() in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1974846#M42130</link>
    <description>&lt;P&gt;When executing the function phNfcLib_Init(), it will return PH_STATUS_INPROCESS a couple of times at first, and when proceeding further, it will return PH_ERR_ABORTED The configuration of the lpTMR module is as follows&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhouwe35_0-1729059305368.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304926i22230B718070D77A/image-size/medium?v=v2&amp;amp;px=400" alt="zhouwe35_0-1729059305368.png" title="zhouwe35_0-1729059305368.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 16 Oct 2024 06:16:14 GMT</pubDate>
    <dc:creator>zhouwe35</dc:creator>
    <dc:date>2024-10-16T06:16:14Z</dc:date>
    <item>
      <title>Initialize NfcLib_Init()</title>
      <link>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1974846#M42130</link>
      <description>&lt;P&gt;When executing the function phNfcLib_Init(), it will return PH_STATUS_INPROCESS a couple of times at first, and when proceeding further, it will return PH_ERR_ABORTED The configuration of the lpTMR module is as follows&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zhouwe35_0-1729059305368.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304926i22230B718070D77A/image-size/medium?v=v2&amp;amp;px=400" alt="zhouwe35_0-1729059305368.png" title="zhouwe35_0-1729059305368.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 06:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1974846#M42130</guid>
      <dc:creator>zhouwe35</dc:creator>
      <dc:date>2024-10-16T06:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: Initialize NfcLib_Init()</title>
      <link>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1975499#M42176</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/241799"&gt;@zhouwe35&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please provide more details on your setup? What is the device you are using?&lt;/P&gt;
&lt;P&gt;Also, are you using the &lt;A href="https://www.nxp.com/design/design-center/development-boards-and-designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY" target="_blank"&gt;NFC Reader Library&lt;/A&gt;? If so, what is the version you are using?&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 21:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1975499#M42176</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-10-16T21:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: Initialize NfcLib_Init()</title>
      <link>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1975577#M42179</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;SPAN&gt;Eduardo&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thank you for your reply, I use window for my device, now I am porting NFC Reader Library on other MCUs, the version is aNfcRdLib_SDK_Evaluation_v2.32, the chip I choose is 3321, I have already configured the required spi communication pins, Reset and interrupt pins in the MCU, but when I execute Figure 1, phNfcLib_Init(), I can see that it is a good choice for me. can I trouble you to help see if there is any problem, or the pin configuration of the side to be What rules should I follow?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;图1&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;图2&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;图3&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;图4&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 16:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1975577#M42179</guid>
      <dc:creator>zhouwe35</dc:creator>
      <dc:date>2024-10-17T16:36:19Z</dc:date>
    </item>
    <item>
      <title>Re: Initialize NfcLib_Init()</title>
      <link>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1976242#M42234</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I just sent you a private Community message.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Oct 2024 16:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Initialize-NfcLib-Init/m-p/1976242#M42234</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-10-17T16:39:58Z</dc:date>
    </item>
  </channel>
</rss>