<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックEIM registers cannot be accessed</title>
    <link>https://community.nxp.com/t5/S32K/EIM-registers-cannot-be-accessed/m-p/1973334#M42040</link>
    <description>&lt;P&gt;When I try to inject faults using EIM, whenever the code accesses the EIM register (read or write), it will enter BusFault. At the same time, when I use the Jtag simulator to observe, I find that EIM is not read, while other registers are OK. Is there any special operation required when accessing the EIM register? I checked RM and I think I meet these conditions. Why can't even the debugger see the register value?&lt;/P&gt;</description>
    <pubDate>Mon, 14 Oct 2024 12:11:57 GMT</pubDate>
    <dc:creator>Janeting123</dc:creator>
    <dc:date>2024-10-14T12:11:57Z</dc:date>
    <item>
      <title>EIM registers cannot be accessed</title>
      <link>https://community.nxp.com/t5/S32K/EIM-registers-cannot-be-accessed/m-p/1973334#M42040</link>
      <description>&lt;P&gt;When I try to inject faults using EIM, whenever the code accesses the EIM register (read or write), it will enter BusFault. At the same time, when I use the Jtag simulator to observe, I find that EIM is not read, while other registers are OK. Is there any special operation required when accessing the EIM register? I checked RM and I think I meet these conditions. Why can't even the debugger see the register value?&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 12:11:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EIM-registers-cannot-be-accessed/m-p/1973334#M42040</guid>
      <dc:creator>Janeting123</dc:creator>
      <dc:date>2024-10-14T12:11:57Z</dc:date>
    </item>
    <item>
      <title>Re: EIM registers cannot be accessed</title>
      <link>https://community.nxp.com/t5/S32K/EIM-registers-cannot-be-accessed/m-p/1974233#M42088</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The reason is simple. You do not have clocks enabled for EIM in your uC.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_0-1728991544468.png" style="width: 971px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304784i667209222CF9A11B/image-dimensions/971x443?v=v2" width="971" height="443" role="button" title="petervlna_0-1728991544468.png" alt="petervlna_0-1728991544468.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please refer to the reference manual: chapter 46.1.5 Peripheral clock gating&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="petervlna_1-1728991597411.png" style="width: 646px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304785i1FF0183ED0202B7A/image-dimensions/646x341?v=v2" width="646" height="341" role="button" title="petervlna_1-1728991597411.png" alt="petervlna_1-1728991597411.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Oct 2024 11:27:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EIM-registers-cannot-be-accessed/m-p/1974233#M42088</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-10-15T11:27:07Z</dc:date>
    </item>
  </channel>
</rss>