<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックAN12218SW java GUI Bootloader diagram</title>
    <link>https://community.nxp.com/t5/S32K/AN12218SW-java-GUI-Bootloader-diagram/m-p/1973287#M42036</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the same problem ( &lt;SPAN&gt;Can't load IA 32-bit .dll on a AMD 64-bit platform)&amp;nbsp;&lt;/SPAN&gt;that was already some discussions regarding the GUI for UART bootloader:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MCU-Bootloader/Unable-to-run-AN12218SW-Bootloader-because-of-32-bit-dll/m-p/977477" target="_blank"&gt;Unable to run AN12218SW Bootloader (because of 32 bit dll) - NXP Community&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I have a business laptop and IT department doesn't allow to install whatever I want and that's why I am not allow to install the old version of java&lt;/P&gt;&lt;P&gt;Because of this issue I want to create my custom GUI for bootloader. Is there any diagram or steps that I should when creating my interface? I saw in S32 Platform that the uC is answering sometimes with "0x41" or "0x45". How should my application interpret all those messages?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
    <pubDate>Mon, 14 Oct 2024 10:50:41 GMT</pubDate>
    <dc:creator>mcristian</dc:creator>
    <dc:date>2024-10-14T10:50:41Z</dc:date>
    <item>
      <title>AN12218SW java GUI Bootloader diagram</title>
      <link>https://community.nxp.com/t5/S32K/AN12218SW-java-GUI-Bootloader-diagram/m-p/1973287#M42036</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have the same problem ( &lt;SPAN&gt;Can't load IA 32-bit .dll on a AMD 64-bit platform)&amp;nbsp;&lt;/SPAN&gt;that was already some discussions regarding the GUI for UART bootloader:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MCU-Bootloader/Unable-to-run-AN12218SW-Bootloader-because-of-32-bit-dll/m-p/977477" target="_blank"&gt;Unable to run AN12218SW Bootloader (because of 32 bit dll) - NXP Community&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I have a business laptop and IT department doesn't allow to install whatever I want and that's why I am not allow to install the old version of java&lt;/P&gt;&lt;P&gt;Because of this issue I want to create my custom GUI for bootloader. Is there any diagram or steps that I should when creating my interface? I saw in S32 Platform that the uC is answering sometimes with "0x41" or "0x45". How should my application interpret all those messages?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 14 Oct 2024 10:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN12218SW-java-GUI-Bootloader-diagram/m-p/1973287#M42036</guid>
      <dc:creator>mcristian</dc:creator>
      <dc:date>2024-10-14T10:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: AN12218SW java GUI Bootloader diagram</title>
      <link>https://community.nxp.com/t5/S32K/AN12218SW-java-GUI-Bootloader-diagram/m-p/1975013#M42153</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I think the information you are looking for can be found in the Application Note, more specifically in chapter 2.2.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12218.pdf" target="_blank"&gt;AN12218: S32K1xx Bootloader – Application Note (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 16 Oct 2024 08:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/AN12218SW-java-GUI-Bootloader-diagram/m-p/1975013#M42153</guid>
      <dc:creator>nxp52415</dc:creator>
      <dc:date>2024-10-16T08:59:19Z</dc:date>
    </item>
  </channel>
</rss>