<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [S32K11x] Questions about the function difference between FTM0 and FTM1 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K11x-Questions-about-the-function-difference-between-FTM0-and/m-p/1971957#M41941</link>
    <description>&lt;P&gt;Dear NXP experts,&lt;/P&gt;&lt;P&gt;As the table shows in the RM,&amp;nbsp; I've some questions:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GavinLi1_0-1728631128045.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304170i881B3D988BE58028/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GavinLi1_0-1728631128045.png" alt="GavinLi1_0-1728631128045.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;GavinLi1_0-1728631128045.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Q1. Only FTM0 can output PMW but FTM1 not?&lt;/P&gt;&lt;P&gt;Q2. If I want to do the motor control, only FTM0 can be used, but FTM1 not support that, right?&lt;/P&gt;&lt;P&gt;Q3. Only FTM1 support input capture, but FTM0 not, right?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Gavin&lt;/P&gt;</description>
    <pubDate>Fri, 11 Oct 2024 07:36:47 GMT</pubDate>
    <dc:creator>GavinLi1</dc:creator>
    <dc:date>2024-10-11T07:36:47Z</dc:date>
    <item>
      <title>[S32K11x] Questions about the function difference between FTM0 and FTM1</title>
      <link>https://community.nxp.com/t5/S32K/S32K11x-Questions-about-the-function-difference-between-FTM0-and/m-p/1971957#M41941</link>
      <description>&lt;P&gt;Dear NXP experts,&lt;/P&gt;&lt;P&gt;As the table shows in the RM,&amp;nbsp; I've some questions:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="GavinLi1_0-1728631128045.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304170i881B3D988BE58028/image-size/medium?v=v2&amp;amp;px=400" role="button" title="GavinLi1_0-1728631128045.png" alt="GavinLi1_0-1728631128045.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;GavinLi1_0-1728631128045.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Q1. Only FTM0 can output PMW but FTM1 not?&lt;/P&gt;&lt;P&gt;Q2. If I want to do the motor control, only FTM0 can be used, but FTM1 not support that, right?&lt;/P&gt;&lt;P&gt;Q3. Only FTM1 support input capture, but FTM0 not, right?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Fri, 11 Oct 2024 07:36:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K11x-Questions-about-the-function-difference-between-FTM0-and/m-p/1971957#M41941</guid>
      <dc:creator>GavinLi1</dc:creator>
      <dc:date>2024-10-11T07:36:47Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K11x] Questions about the function difference between FTM0 and FTM1</title>
      <link>https://community.nxp.com/t5/S32K/S32K11x-Questions-about-the-function-difference-between-FTM0-and/m-p/1972331#M41963</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;With all FTM modules you can perform all modes described in &lt;EM&gt;Table 47-5. Channel Modes Selection&lt;/EM&gt;.&lt;/P&gt;
&lt;P&gt;FTM modulation, Quadrature Decoder, Hall sensor support and Dithering are particular modes that are only available in some FTM modules, like is described in &lt;EM&gt;Table 47-1. FTM instances and features&lt;/EM&gt;. For these modes you can refer to their respective section in FTM chapter of reference manual.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Fri, 11 Oct 2024 19:02:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K11x-Questions-about-the-function-difference-between-FTM0-and/m-p/1972331#M41963</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2024-10-11T19:02:52Z</dc:date>
    </item>
  </channel>
</rss>