<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックStrange error in Gpt plugin</title>
    <link>https://community.nxp.com/t5/S32K/Strange-error-in-Gpt-plugin/m-p/1971384#M41900</link>
    <description>&lt;P&gt;I'm trying to work on&amp;nbsp;S32K3_BJB777A_4.4_R21-11_0.8.0_CD04_D2404 example which has a Phy_665a plugin that I need to work on. For this example, I have installed following (in that sequence):&lt;/P&gt;&lt;P&gt;EB Tresos Studio 29.0.0&lt;/P&gt;&lt;P&gt;SW32K3_RTD_4.4_R21-11_3.0.0&lt;/P&gt;&lt;P&gt;SW32K3_BMS_SDK_4.4_R21-11_1.0.2&lt;/P&gt;&lt;P&gt;SW32K3_BMS_GEN1_SL_SDK_4.4_R21-11_1.0.3_DEMO&lt;/P&gt;&lt;P&gt;S32K3_BJB777A_4.4_R21-11_0.8.0_CD04_D2404&lt;/P&gt;&lt;P&gt;An then copied the required plugins to EB Tresos plugins folder.&lt;/P&gt;&lt;P&gt;After this I added&amp;nbsp;BJB777A example project in EB Tresos and without making any change, just tried Verify and Generate options. During Verify, it threw an error: Invalid XPath expression for attribute "RANGE", pointing to Gpt plugin.&lt;/P&gt;&lt;P&gt;When I checked the required range of GptChannelTickFrequency (0 -&amp;gt; 9223372036854775807), the default value of 8.0E7 is clearly within the range.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What could be going wrong with the Gpt here ?&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="MC33665A" id="MC33665A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;#MC3377&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sbadave_0-1728564533551.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304017i5C4E095C96666849/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sbadave_0-1728564533551.png" alt="sbadave_0-1728564533551.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Oct 2024 12:49:27 GMT</pubDate>
    <dc:creator>sbadave</dc:creator>
    <dc:date>2024-10-10T12:49:27Z</dc:date>
    <item>
      <title>Strange error in Gpt plugin</title>
      <link>https://community.nxp.com/t5/S32K/Strange-error-in-Gpt-plugin/m-p/1971384#M41900</link>
      <description>&lt;P&gt;I'm trying to work on&amp;nbsp;S32K3_BJB777A_4.4_R21-11_0.8.0_CD04_D2404 example which has a Phy_665a plugin that I need to work on. For this example, I have installed following (in that sequence):&lt;/P&gt;&lt;P&gt;EB Tresos Studio 29.0.0&lt;/P&gt;&lt;P&gt;SW32K3_RTD_4.4_R21-11_3.0.0&lt;/P&gt;&lt;P&gt;SW32K3_BMS_SDK_4.4_R21-11_1.0.2&lt;/P&gt;&lt;P&gt;SW32K3_BMS_GEN1_SL_SDK_4.4_R21-11_1.0.3_DEMO&lt;/P&gt;&lt;P&gt;S32K3_BJB777A_4.4_R21-11_0.8.0_CD04_D2404&lt;/P&gt;&lt;P&gt;An then copied the required plugins to EB Tresos plugins folder.&lt;/P&gt;&lt;P&gt;After this I added&amp;nbsp;BJB777A example project in EB Tresos and without making any change, just tried Verify and Generate options. During Verify, it threw an error: Invalid XPath expression for attribute "RANGE", pointing to Gpt plugin.&lt;/P&gt;&lt;P&gt;When I checked the required range of GptChannelTickFrequency (0 -&amp;gt; 9223372036854775807), the default value of 8.0E7 is clearly within the range.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What could be going wrong with the Gpt here ?&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="MC33665A" id="MC33665A"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;#MC3377&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="sbadave_0-1728564533551.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304017i5C4E095C96666849/image-size/medium?v=v2&amp;amp;px=400" role="button" title="sbadave_0-1728564533551.png" alt="sbadave_0-1728564533551.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 12:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Strange-error-in-Gpt-plugin/m-p/1971384#M41900</guid>
      <dc:creator>sbadave</dc:creator>
      <dc:date>2024-10-10T12:49:27Z</dc:date>
    </item>
  </channel>
</rss>