<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: External oscillator before FXOSC configuration in S32K</title>
    <link>https://community.nxp.com/t5/S32K/External-oscillator-before-FXOSC-configuration/m-p/1971196#M41893</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Sorry. Since S32K3XXRM has clearly mentioned the following requirements, I'm afraid you can only follow the instructions:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;28.1.1 Chip-specific FXOSC information
For bypass mode applications, the EXTAL pin should be driven low when FXOSC is in off/disabled state.
•While initializing FXOSC: When the FXOSC is used in Bypass mode, the external clock source can only be enabled after the FXOSC is enabled.
•While disabling FXOSC: When the FXOSC is used in Bypass mode, the external clock source must already be inactive before disabling the FXOSC.&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Oct 2024 08:47:57 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2024-10-10T08:47:57Z</dc:date>
    <item>
      <title>External oscillator before FXOSC configuration</title>
      <link>https://community.nxp.com/t5/S32K/External-oscillator-before-FXOSC-configuration/m-p/1969305#M41804</link>
      <description>&lt;P&gt;I am trying to use an external quartz oscillator with an S32K344, instead of using a standalone quartz crystal.&amp;nbsp; The reference manual notes, "When the FXOSC is used in Bypass mode, the external clock source can only be enabled after the FXOSC is enabled."&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does this mean that, with a 4-pin oscillator where one of the pins is an enable pin, I need to use a GPIO to not enable the oscillator until FXOSC is enabled (OSCON is set) and in bypass mode? I would instead prefer to hardwire the oscillator to always be enabled, what will happen if a clock is provided to EXTAL before FXOSC is enabled and put into bypass mode?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Oct 2024 22:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/External-oscillator-before-FXOSC-configuration/m-p/1969305#M41804</guid>
      <dc:creator>via</dc:creator>
      <dc:date>2024-10-08T22:47:57Z</dc:date>
    </item>
    <item>
      <title>Re: External oscillator before FXOSC configuration</title>
      <link>https://community.nxp.com/t5/S32K/External-oscillator-before-FXOSC-configuration/m-p/1971196#M41893</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Sorry. Since S32K3XXRM has clearly mentioned the following requirements, I'm afraid you can only follow the instructions:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;28.1.1 Chip-specific FXOSC information
For bypass mode applications, the EXTAL pin should be driven low when FXOSC is in off/disabled state.
•While initializing FXOSC: When the FXOSC is used in Bypass mode, the external clock source can only be enabled after the FXOSC is enabled.
•While disabling FXOSC: When the FXOSC is used in Bypass mode, the external clock source must already be inactive before disabling the FXOSC.&lt;/LI-CODE&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 08:47:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/External-oscillator-before-FXOSC-configuration/m-p/1971196#M41893</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-10-10T08:47:57Z</dc:date>
    </item>
  </channel>
</rss>