<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Guidance for Basic PWM Configuration on NXP S32K312</title>
    <link>https://community.nxp.com/t5/S32K/Guidance-for-Basic-PWM-Configuration-on-NXP-S32K312/m-p/1970013#M41856</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if you have RTD installed then you can refer to basic PWM example called "Emios_Pwm_Ip_Example_S32K344" using low level driver or&amp;nbsp;Pwm_example_S32K344 using MCAL level driver. If interesting in high level driver usage below thread can be very useful as well;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-MCAL-K344-KEY-control-EMIOS-PWM/ta-p/1967347" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-MCAL-K344-KEY-control-EMIOS-PWM/ta-p/1967347&lt;/A&gt;&lt;BR /&gt;And a recommendation is to read eMIOS chapter of the device RM for implementation info, available modes functionality etc.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
    <pubDate>Wed, 09 Oct 2024 13:31:30 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-10-09T13:31:30Z</dc:date>
    <item>
      <title>Guidance for Basic PWM Configuration on NXP S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Guidance-for-Basic-PWM-Configuration-on-NXP-S32K312/m-p/1969915#M41848</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hello NXP Community,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I'm new to working with the S32K312 microcontroller and I'm trying to generate a basic PWM signal using the eMIOS module. I'm using S32 Design Studio and would appreciate any guidance or example code to get started with PWM generation.&lt;/P&gt;&lt;H3&gt;&lt;STRONG&gt;My Setup&lt;/STRONG&gt;:&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;STRONG&gt;MCU&lt;/STRONG&gt;: S32K312&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Tool&lt;/STRONG&gt;: S32 Design Studio&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;PWM Module&lt;/STRONG&gt;: eMIOS&lt;/LI&gt;&lt;LI&gt;&lt;STRONG&gt;Instance/Channel&lt;/STRONG&gt;: Any basic example will do.&lt;/LI&gt;&lt;/UL&gt;&lt;H3&gt;&lt;STRONG&gt;Questions&lt;/STRONG&gt;:&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;Can anyone share a simple code example with configuration or guide to configure and generate a PWM signal on the S32K312 using the eMIOS module?&lt;/LI&gt;&lt;LI&gt;What are the key steps or important parameters to keep in mind while setting up PWM?&lt;/LI&gt;&lt;LI&gt;Are there any existing tutorials or application notes that I can refer to for PWM configuration on this MCU?&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;HR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 11:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Guidance-for-Basic-PWM-Configuration-on-NXP-S32K312/m-p/1969915#M41848</guid>
      <dc:creator>Mohmedsohel</dc:creator>
      <dc:date>2024-10-09T11:56:06Z</dc:date>
    </item>
    <item>
      <title>Re: Guidance for Basic PWM Configuration on NXP S32K312</title>
      <link>https://community.nxp.com/t5/S32K/Guidance-for-Basic-PWM-Configuration-on-NXP-S32K312/m-p/1970013#M41856</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;if you have RTD installed then you can refer to basic PWM example called "Emios_Pwm_Ip_Example_S32K344" using low level driver or&amp;nbsp;Pwm_example_S32K344 using MCAL level driver. If interesting in high level driver usage below thread can be very useful as well;&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-MCAL-K344-KEY-control-EMIOS-PWM/ta-p/1967347" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/RTD400-MCAL-K344-KEY-control-EMIOS-PWM/ta-p/1967347&lt;/A&gt;&lt;BR /&gt;And a recommendation is to read eMIOS chapter of the device RM for implementation info, available modes functionality etc.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 13:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Guidance-for-Basic-PWM-Configuration-on-NXP-S32K312/m-p/1970013#M41856</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-10-09T13:31:30Z</dc:date>
    </item>
  </channel>
</rss>